Post Go back to editing

my endpoint is not acting immediately on CP commands

In my basic ADRadioNet evaluation demo (with CP => R => EP), the commands I sent from the CenterPoint are not immediately reaching the endpoint. Is there something wrong with the way I am sending these commands?. I expect the EP to respond right away without any delay.

Parents
  • Thanks. My last question was not related to Fragementation but it is good to know that the protocol doesn't use fragmentation.

    My quesiton was for a case where R1 is not reachable when EP sends Message 2(may be due to change in network conditions) and if another Rotuer R2 on a different downlink channel forwards this message to the CP. As command 1 was buffered at R1 does the CP identify that a different router was used this time and retransmitt Command 1 to R2 or Command 1 will be delivered to EP only when the next timer EP uses R1 for forwarding a message to CP.

Reply
  • Thanks. My last question was not related to Fragementation but it is good to know that the protocol doesn't use fragmentation.

    My quesiton was for a case where R1 is not reachable when EP sends Message 2(may be due to change in network conditions) and if another Rotuer R2 on a different downlink channel forwards this message to the CP. As command 1 was buffered at R1 does the CP identify that a different router was used this time and retransmitt Command 1 to R2 or Command 1 will be delivered to EP only when the next timer EP uses R1 for forwarding a message to CP.

Children
No Data