Post Go back to editing

How to recover the setting on EV-ADRN-WSN-1Z

Hi Sir,

      First, I got the ADRN-WSN-1Z and the function is ok , but when one of colleague do some change on AnodeCoding and the problem happen. Although the main board still could be saw on PC, the data of Bunck WSN board can’t be read on  AnodeCenterPoint(seem doesn't connect to Main board but the LED light in the first time when power on). I try to follow the User guide to back default setting . but it’s not work. Is there any suggestion in this to make it work?  

Parents
  • Hi Kun-jing,

    I presume the configuration screenshot you posted is for the EVAL-ADuCRF101-MK board. On the similar lines we need to check the configuration of other nodes like Endpoint (BUNCH). Follow the below mentioned instructions to capture this information.

    • Make sure the 3V button battery is inserted in battery slot B1 of BUNCH board.
    • Connect the BUNCH board to PC via USB-SWD/UART-EMUZ interface board using USB cables as shown below.

      7635.2b70e782e18b24ffb7fcfa25e5d4605f.png

    • Make sure the links A, B & C of LK2 are shorted using jumpers.

    After connecting the BUNCH (EndPoint) to PC open the ANodeConfiguration tool and click on “Find devices” button to detect the device. Once EndPoint is detected select the end point and then click on the “Get config” button to read configuration from the device.

    Please refer to the “ANODE CONFIG GUI” section from User Guide-ADRN-WSN-1.pdf for detecting, configuring a device and more information.

    With the CenterPoint configuration you have posted, to establish communication the EndPoint should have the configuration as shown below. Please try configuring the Endpoint with the below configuration.

    5808.7893a92252c9c04eb44c78aff1850773.png

Reply
  • Hi Kun-jing,

    I presume the configuration screenshot you posted is for the EVAL-ADuCRF101-MK board. On the similar lines we need to check the configuration of other nodes like Endpoint (BUNCH). Follow the below mentioned instructions to capture this information.

    • Make sure the 3V button battery is inserted in battery slot B1 of BUNCH board.
    • Connect the BUNCH board to PC via USB-SWD/UART-EMUZ interface board using USB cables as shown below.

      7635.2b70e782e18b24ffb7fcfa25e5d4605f.png

    • Make sure the links A, B & C of LK2 are shorted using jumpers.

    After connecting the BUNCH (EndPoint) to PC open the ANodeConfiguration tool and click on “Find devices” button to detect the device. Once EndPoint is detected select the end point and then click on the “Get config” button to read configuration from the device.

    Please refer to the “ANODE CONFIG GUI” section from User Guide-ADRN-WSN-1.pdf for detecting, configuring a device and more information.

    With the CenterPoint configuration you have posted, to establish communication the EndPoint should have the configuration as shown below. Please try configuring the Endpoint with the below configuration.

    5808.7893a92252c9c04eb44c78aff1850773.png

Children
No Data