Post Go back to editing

Prolem with ADuCRF101MK, I don't see the bunch on AnodeCenterPoint

I have wsn quicksrart kit for ADuCRF101MK. When I open AnodeCenterPoint the program found the device but when i turn on the accelerometer it doesn't see nothing. I try to change the configuaration but nothing. I went to AndeConfiguration and I connect the bunch wsn to j-link and I configured the bunch with end point after i connected ADu.. but nothing. Anodecenterpoint see only ADu...and doesn't see my sensor. Can you hel me? thank you

Parents
  • Hi,

    I presume you are using the EV-ADRN-WSN-1Z kit with the ADRadioNet EDKv2.0 version of binaries for the demo setup. The EV-ADRN-WSN-1Z kit contains the following hardware

    1. EV-ADRN-WSN-1Z (2 BUNCH WSN modules + 1 EVAL-ADuCRF101MK)

    2. USB-SWD/UART -EMUZ module - 1 min.


    Please ensure your configuration is correct. Provide me the following information

      • Version of the binaries used on both the EndPoint and CenterPoint
      • Mode of powering the EndPoint (battery or USB-SWD/UART-EMUZ)
      • Share the screenshots of the ANodeConfig tool for both EndPoint and CenterPoint displaying configuration.

    If you are not able to detect the EndPoint on the ANodeConfig tool please erase and flash the node with the binaries once again using CM3WSD (use Flash Action as Mass Erase to erase the boards) provided with the package. Refer to “ADRN01-All-in-One-GettingStartedGuide_v2.0” provided along with the package for how to flash the binaries using CM3WSD.

    The issue of EndPoint not detecting after the configuration is addressed in the following post please follow the below link.

                            https://ez.analog.com/thread/71542

    Thanks,

    Harish

Reply
  • Hi,

    I presume you are using the EV-ADRN-WSN-1Z kit with the ADRadioNet EDKv2.0 version of binaries for the demo setup. The EV-ADRN-WSN-1Z kit contains the following hardware

    1. EV-ADRN-WSN-1Z (2 BUNCH WSN modules + 1 EVAL-ADuCRF101MK)

    2. USB-SWD/UART -EMUZ module - 1 min.


    Please ensure your configuration is correct. Provide me the following information

      • Version of the binaries used on both the EndPoint and CenterPoint
      • Mode of powering the EndPoint (battery or USB-SWD/UART-EMUZ)
      • Share the screenshots of the ANodeConfig tool for both EndPoint and CenterPoint displaying configuration.

    If you are not able to detect the EndPoint on the ANodeConfig tool please erase and flash the node with the binaries once again using CM3WSD (use Flash Action as Mass Erase to erase the boards) provided with the package. Refer to “ADRN01-All-in-One-GettingStartedGuide_v2.0” provided along with the package for how to flash the binaries using CM3WSD.

    The issue of EndPoint not detecting after the configuration is addressed in the following post please follow the below link.

                            https://ez.analog.com/thread/71542

    Thanks,

    Harish

Children
No Data

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.