I have ev adrn wsn 1z and I save the data with a particular program in c, but I can't see the data in real time and I have to wait after for creating the graphic.
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
I have ev adrn wsn 1z and I save the data with a particular program in c, but I can't see the data in real time and I have to wait after for creating the graphic.
Hi,
The purpose of this community is to provide help and support on ADRadioNet evaluation demo bring-up. Beyond this it’s up to you on how you want to create your application. But I am curious to find out what you are doing as I understand you are able to save the data using a C-program. Can you provide the following details.
Thanks
Harish
I use the program serial monitor and save the hexdecimal data into a file, after I have created a program in c that extract the hexdecimal data of the axes x, y, z. I save this data into 3 different file. Now I have to convert this data in decimal and I use excel with a macro, and I create tre colum of data, finally I create a graphic. Now I'm studing for creating a graphic in real time.
the sleep time is on 20ms but anode center point write only 12 data at 1 second. Anode center point with this sleep time, write uart error on uart status. For me is import to see graphic in real time with the minimum sleep time. I know that 20ms sleep time is not real, but for me is importat reduce this time.
Hi
So you are doing an offline plotting from the sensor data that you are receiving on the CenterPoint. You can create your own mechanisms to plot the sensor data and that is outside the scope of this support. But I want to share a news that there is new release that will go live (in ~2weeks) with a new and enhanced PC tool. This will have a form of real-time plotting of sensor data, hopefully it is useful for you. Please stay tuned on this.
On the other question: The minimum sleep time that can be configured using ANodeConfig tool is 1 second. Since the ADRadioNet devices are intended for low power and battery operated, most of the time the devices are expected to be in sleep state. An option for user with 250 milliseconds sleep time is provided in the form of command (please refer to “ANodeCenterPoint: Control & Monitoring:” section of ADRN01-All-in-One-GettingStartedGuide_v2.0). Please note, the support from this forum is limited to evaluating the solution as-is and for any new feature requirements to build a new product you have to reach out to local ADI sales team.
thanks
Harish