The following table shows the operating modes, corresponding data rates and number of channels that are supported in AD6LoWPAN solution.
The maximum data rate that is supported currently is 100kbps. The frequency bands and the data rates are according to IEEE 802.15.4g specification.
The user does not have the control to modify these values as these are configured internally based on the frequency band and the PHY_MODE selected by the user from the ADWSN-UI-Tool.
S.No
ISM Band Supported
Operating Mode & Data Rate
Number of Channels
1
863–870 (Europe)
Mode 1 50 kbps 2FSK
17
Mode 2 100 kbps 2FSK
2
896–901 (U.S. FCC Part 90)
Mode 1 10 kbps 2FSK
255
Mode 2 20 kbps 2FSK
Mode 3 40 kbps 2FSK
3
901–902 (U.S. FCC Part 24)
73
4
902–928 (U.S. ISM)
64
5
917–923.5 (Korea)
32
6
928–960b (U.S. FCC Part 22/24/90/101)
7
920-928 (Japan)
18
8
950-958 (Japan)
16
This FAQ was generated from the following discussion: What data rates are supported in AD6LoWPAN and what is the maximum data rate supported?