Data corresponding to how many number of sensors is displayed in the ADWSN UI tool?
What if I want interface more sensors in my design, how would I be able to visualize this data from new/additional sensors?
Data corresponding to how many number of sensors is displayed in the ADWSN UI tool?
What if I want interface more sensors in my design, how would I be able to visualize this data from new/additional sensors?
The ADWSN UI tool is an evaluation tool that displays data from the 4 on-board sensors.
The WSN BUNCH boards has following four sensors are mounted on board.
| On-board Sensor | Description |
|---|---|
ADT75 |
Temperature Sensor |
| ADXL362 | Accelerometer |
| SHT21 | Temperature and Relative Humidity Sensor |
| ADPS9005 | Ambient Light Sensor |
The figure below displays the sensors data plotting that is supported in this evaluation package.
7674.eb7ed9aaacaf57b0de48dace4d046f25.jpg
When additional sensors are interfaced in the new design, then user will be able to still use this tool without plotting. Such data can be visualized in the Network Overview window.