Post Go back to editing

Device types in AD6LoWPAN EDK?

What are the different types of devices supported in AD6LoWPAN EDK? Can you explain the functionality very briefly?

  • AD6LoWPAN uses the following 3 types of devices in a typical network. The last device is for sniffing over the air packets.

    • 6LoWPAN Border Router (6LBR):
      • Border router at the edge of separate LoWPANs or a LoWPAN and another IP network, responsible for IPv6 prefix propagation within the LoWPAN. Usually the data concentrator for all the data in a PAN.
    • 6LoWPAN Node (6LN):
      • Sensor node which acts as a RPL leaf node in a 6LoWPAN Network. Collects data from sensors and transmits to border router (directly or via router/s).
    • 6LoWPAN Router (6LR):
      • An intermediate router in the LoWPAN that communicates with other 6LRs in the same LoWPAN; only in route-over topologies. A router with UDP enabled, can act as sensor mote along with the routing functionality.
    • 6LoWPAN Sniffer (6LSN):
      • This captures all the packets in a particular channel. Useful in debugging/network monitoring.
      • The sniffer is an optional device type which can be prepared by the user to monitor the network in a particular channel using wireshark tool.
  • This question has been closed by the EZ team and is assumed answered.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.