Article What is the default tx power in AD6LoWPAN EDKv1.0, and how do I change it?

Original Question: What is the default tx power in AD6LoWPAN EDKv1.0, and how do I change it? by NagarjunaG

What is the default transmit power used in AD6LoWPAN EDKv1.0?

How do I change it to experiment more with my network?


Verified Answer: RE: What is the default tx power in AD6LoWPAN EDKv1.0, and how do I change it? by NagarjunaG

The default transmit power in the Sub-GHz radio transceiver of ADuCRF101 part is 13.5dBm with single ended power amplifier, and 10dBm with differential power amplifier. All the devices (Edge Router, Router, and Host) in the EDK are preset with the value of 63 corresponding to this maximum PA (power amplification) in the Sub-GHz radio as explained above.

The Tx Power option is provided in the ADWSN-UI tool and user can decrease or increase the transmit power level in steps as below:



Question: RE: What is the default tx power in AD6LoWPAN EDKv1.0, and how do I change it? by ezadminThis question has been closed by the EZ team and is assumed answered.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.