Article Default configuration for AD6LoWPAN devices

Original Question: Default configuration for AD6LoWPAN devices by NagarjunaG

My devices are not working. How do I get back the factory default configuration of a device? What are the default configurations used in the demo setup for each of the devices?


Verified Answer: RE: Default configuration for AD6LoWPAN devices by NagarjunaG

The default configuration for any AD6LoWPAN device can be obtained by clicking the “Factory Default” button in the Configuration window of ADWSN-UI tool. Once the device is detected, select that device and click “Factory Default” tab as shown below.

If you load the firmware afresh on the device and bring it up, it comes up with the factory default configuration. The user then can configure the device manually as desired.

 

The default configuration parameters used in the AD6LoWPAN demo setup are as shown below:

 

Attribute

Default Value

Remark

MAC Address

6LBR     : 0x0005f7feff000001

6LR        : 0x0005f7feff000002

6LN       : 0x0005f7feff000003

Unique IEEE Address used by device for communication

ISMBand

ISMBAND_863_870MHZ

Operating frequency band

PHY

Operating Mode 1:  50 kbps  2FSK

Operating data rate and modulation

Channel

0

Operating channel

Tx Power

63

Transmit Power

Sleep Time

1 (Applicable only for Nodes)

Node’s periodic sleep time in seconds.

Orbit

1 (Applicable only for Nodes and Routers)

Specifies the parent’s orbit at which the node shall attempt to join.


Question: RE: Default configuration for AD6LoWPAN devices by ezadminThis question has been closed by the EZ team and is assumed answered.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.