Article Key features & Product details of AD6LoWPAN EDKv1.0

Original Question: Key features & Product details of AD6LoWPAN EDKv1.0 by NagarjunaG

What is AD6LoWPAN EDKv1.0? What are the key features & product details of this solution?


Verified Answer: RE: Key features & Product details of AD6LoWPAN EDKv1.0 by NagarjunaG

AD6LoWPAN EDKv1.0 is Evaluation Development Kit that includes complete source code and required software tools to quickly evaluate Analog Devices 6LoWPAN wireless sensor network solution on ADuCRF101 evaluation hardware platforms (www.analog.com/wsn).

 

The solution is based on Contiki lightweight sensor OS. The starting point for AD6LoWPAN solution is uIPv6 from Contiki 2.5 as the key constituent. On top of this, Analog Devices upgraded the stack with the following RFC's ..

  • RFC 6550: RPL: IPv6 Routing Protocol for Low Power and Lossy Network
  • RFC 6282: Compression Format for IPv6 Datagrams over IEEE 802.15.4 based networks
  • RFC 6775: Neighbor Discovery Optimization for IPv6 over Low Power Wireless Personal Area Networks

AD6LoWPAN EDKv1.0 Features:

  • Easy to Deploy: IPv6  Address & Prefix auto configuration, Neighbor Discovery and Auto parent selection eliminates network administration overheads and provide self-healing capabilities.
  • Seamless connectivity: IPv6 networking throughout the mesh, star and tree topologies
  • Robust Interoperable technology: IETF driven standards enables robust multi-vendor interoperable wireless mesh networks
  • Optimum footprint: Enables both communication and application to reside on the same processor, configurable to work with 32, 64 & 128kB flash.
  • Optimized for battery powered devices: Fast network join and application initiated healing and power down options enables using different power profiles based on application requirements.
  • Supported with ADSensorApplication suite: Sample UDP based sensor application code for EV-ADRN-WSN-1Z platform with multiple sensors onboard.
  • Network Visualization, Diagnosis & Troubleshooting: Supports the wireshark tool for sniffing the Over-The-Air (OTA) packets.
  • Optimized data transmission: Supported with in-built Acknowledgement and re-transmission mechanism.


Product Details:

  • All-in-One Getting Started Guide
  • Installer package with click through SLA
  • ADWSN-UI-Tool  (Configure, Monitor the WSN devices, with Quick Demo Wizards)
  • IPv6/6LoWPAN Low Power, Low Footprint stack source code for mesh capable sensor nodes.
  • ADSensorApp source code
  • Sample UDP based sensor application for EV-ADRN-WSN-1Z
  • IAR Project workspace configuration - to build all node types required for setting up an IPv6/6LoWPAN mesh network.
  • Wireshark network packet analyzer adapter (firmware & free PC software)


Question: RE: Key features & Product details of AD6LoWPAN EDKv1.0 by ezadminThis question has been closed by the EZ team and is assumed answered.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.