adrv9008-1 profile TES

Hi:

in  ADRV-9008-1 ,I used device clock as 100MHz to generate  a custom profile.But when I load the profile txt into adrv9008-1's TES , on the gui why the device clock didn't change(only can select 122.88MHz)?  thank you for your answer.

Parents Reply Children
  • Do you mean I have to connect the board to use this software? I just want to use it to generate the init. C file and debug it with the board a few days later.

    I configure VCXO freq to 50MHz and DEV_ CLK to 100MHz, DEV_ CLK is an integral multiple of VCXO freq, but TES still displays DEV_ CLK is 122.88mhz by default but not 100MHz

  • 0
    •  Analog Employees 
    on Oct 21, 2020 7:35 AM 2 months ago in reply to 1135553530@qq.com

    Share with us the config file that you generated from filter wizard using insert option in command window.

  • Rx_BW82_OR100.txt
    <profile Talise version=1 name=Rx_BW82_OR100>
     <clocks>
      <deviceClock_kHz=100000>
      <clkPllVcoFreq_kHz=8000000>
      <clkPllHsDiv=2.0>
     </clocks>
    
     <rx name=Rx 82.00MHz, OutputRate 100.00MHz, TotalDecimation 20>
      <rxChannels=TAL_RX1RX2>
      <rxFirDecimation=2>
      <rxDec5Decimation=5>
      <rhb1Decimation=2>
      <rxOutputRate_kHz=100000>
      <rfBandwidth_Hz=82000000>
      <rxBbf3dBCorner_kHz=100000>
      <rxDdcMode=0>
    
      <rxNcoShifterCfg>
       <bandAInputBandWidth_kHz=0>
       <bandAInputCenterFreq_kHz=0>
       <bandANco1Freq_kHz=0>
       <bandANco2Freq_kHz=0>
       <bandBInputBandWidth_kHz=0>
       <bandBInputCenterFreq_kHz=0>
       <bandBNco1Freq_kHz=0>
       <bandBNco2Freq_kHz=0>
      </rxNcoShifterCfg>
    
      <filter FIR gain_dB=-6 numFirCoefs=72>
      0
      -1
      2
      3
      -5
      -7
      12
      15
      -25
      -29
      46
      53
      -79
      -90
      129
      146
      -200
      -225
      303
      338
      -448
      -500
      637
      718
      -903
      -1028
      1268
      1474
      -1811
      -2175
      2684
      3425
      -4498
      -6831
      9597
      30772
      30772
      9597
      -6831
      -4498
      3425
      2684
      -2175
      -1811
      1474
      1268
      -1028
      -903
      718
      637
      -500
      -448
      338
      303
      -225
      -200
      146
      129
      -90
      -79
      53
      46
      -29
      -25
      15
      12
      -7
      -5
      3
      2
      -1
      0
      </filter>
    
      <rxAdcProfile num=42>
      261
      144
      181
      90
      1280
      366
      1258
      27
      1280
      17
      731
      39
      48
      47
      28
      160
      0
      0
      0
      0
      40
      0
      7
      6
      42
      0
      7
      6
      42
      0
      25
      27
      0
      0
      25
      27
      0
      0
      165
      44
      31
      905
      </rxAdcProfile>
     </rx>
    
     <obsRx name=Rx 200.00MHz, OutputRate 245.76MHz, TotalDecimation 8>
      <obsRxChannelsEnable=TAL_ORXOFF>
      <enAdcStitching=0>
      <rxFirDecimation=2>
      <rxDec5Decimation=4>
      <rhb1Decimation=1>
      <orxOutputRate_kHz=245760>
      <rfBandwidth_Hz=200000000>
      <rxBbf3dBCorner_kHz=225000>
      <orxDdcMode=0>
    
      <filter FIR gain_dB=0 numFirCoefs=48>
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      1
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      </filter>
    
      <orxLowPassAdcProfile num=1>
      0
      </orxLowPassAdcProfile>
    
      <orxBandPassAdcProfile num=1>
      0
      </orxBandPassAdcProfile>
    
     </obsRx>
    
     <lpbk>
      <rxFirDecimation=2>
      <rhb1Decimation=1>
      <outputRate_kHz=245760>
      <rfBandwidth_Hz=220000000>
      <rxBbf3dBCorner_kHz=225000>
    
      <filter FIR gain_dB=0 num=48>
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      1
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      </filter>
    
      <lpbkAdcProfile num=1>
      0
      </lpbkAdcProfile>
     </lpbk>
    
     <tx name=Tx 200.00MHz, InputRate 245.76MHz, TotalInterpolation 32>
      <txChannels=TAL_TXOFF>
      <dacDiv=1>
      <txFirInterpolation=1>
      <thb1Interpolation=2>
      <thb2Interpolation=2>
      <thb3Interpolation=2>
      <txInt5Interpolation=1>
      <txInputRate_kHz=245760>
      <primarySigBandwidth_Hz=75000000>
      <rfBandwidth_Hz=200000000>
      <txDac3dBCorner_kHz=200000>
      <txBbf3dBCorner_kHz=100000>
    
      <filter FIR gain_dB=0 numFirCoefs=20>
      0
      0
      0
      0
      0
      0
      0
      0
      0
      1
      0
      0
      0
      0
      0
      0
      0
      0
      0
      0
      </filter>
     </tx>
    </profile>
    

  • 0
    •  Analog Employees 
    on Oct 21, 2020 12:06 PM 2 months ago in reply to 1135553530@qq.com

    Yes. The DEV_CLK is getting set to 92.16MHz instead of 100MHz. 

    Connect to the board using GUI and load the profile and then generate the initdata.c in online mode.