Hi:
in ADRV-9008-1 ,I used device clock as 100MHz to generate a custom profile.But when I load the profile txt into adrv9008-1's TES , on the gui why the device clock didn't change(only can select 122.88MHz)? thank you for your answer.
The default on board VCXO is 122.88MHz and DEV_CLK frequency should be an integer multiple of that. If you want to use 100MHz DEV_CLK then you have replace the onboard VCXO accordingly to the one that you have set in the filter wizard and then load it into GUI and initialize.
I have set in the wizard and then load it into GUI and initialize, I set device clock 100MHz in the wizard, but it always keep 122.88MHz after load and initialize GUI.
It is strange, When I set the device ADRV9008-2 and setd clock 100MHz, after loading it display 100MHz on the GUI.