TES GUI failed to generate Init .c Files

Hello!

I have a problem to  to generate Init .c Files for Transceiver Evaluation Software for ADRV9008-1.

I have no Zing mother board and perform all manipulations without connection.

  1. I press GUI/Connect and get "Cannot Connect to the Device. Please Check IP Address And/Or Port Number" message.
  2. Configuration/Device set to ADRV9008-1
  3. Press Tools/Create Script/Init .c Files.
  4. Windows explorer appears to save files, but after that  "Error: See Log File for details" message appear in right down corner of the GUI. When I open File/View Log File, Error Log is empty. No any file is saved.

GUI version: 3.6.0.5

.Net version 4.7.2

Windows 7