In the SDK package there is a Changelog.txt file that details all known additions, changes and bugs at the time of release. This page contains a list of SDK and TES Errata found after release, which will be updated as each bug is reported or resolved.
Last Edited: 6th July 2021
Errata | Date logged | SDK version | Fix in SDK |
FPGA source code not included | 31 - Aug - 21 | 17 | 17.1 |
MCS Operation not working | 31 - Aug - 21 | 17 | 17.1 |
Segmentation fault due to large memory allocations on the stack | 1 - June - 21 | 16 | 18 |
MCS profile configuration crashes the TES | 14 - Oct - 21 | 18 | 18.1 |
FPGA source code not included
Bug:
FPGA source code was omitted from the SDK 17 release.
Customer Impact:
Users can download a new release of SDK from the product page (version 17.1) that has the FPGA source code included.
This is fixed in SDK 17.1
MCS Operation not working
Bug:
MCS operation in SDK version 17 did not function as expected and as a result was not useable.
Customer Impact:
Users can download a new release of SDK from the product page (version 17.1) that has resolved this issue.
This is fixed in SDK 17.1
Segmentation fault due to large memory allocations on the stack
Bug:
By default, ADI_FPGA9001_MAX_CAPTURE_BYTES is set to the absolute maximum supported by the FPGA. This may cause a segmentation fault due to large memory allocations on the stack.
Customer Impact:
This can be resolved by either:
Modify the makefile CFLAGS to include -DADI_FPGA9001_USE_DYNAMIC_MEMORY. This makes the ADI_FPGA9001_MAX_CAPTURE_BYTES value irrelevant, instead allocating memory on the heap.
Modify the value of ADI_FPGA9001_MAX_CAPTURE_BYTES to be smaller - ideally only as large as the largest required data capture/transmit
This is fixed in SDK 18
MCS profile configuration crashes the TES
Bug:
When programming a configuration that includes Multi-Chip Synchronization the TES GUI will crash. This is caused by a timer timeout issue in the FW and is currently being looked at.
Customer Impact:
Currently stay using SDK version 17 to test the MCS function. An update will follow shortly to fix this in the SDK 18.
This is fixed in SDK 18.1