Hello.
I use TES 0.20.0 on Windows 10 OS. While experimenting with Automated TDD, I observe that Timing diagrams are not shown in the pop-up window as in Figure 305. Automated TDD Timing Diagram, see screenshot below. Is this a known issue?
Further, I would like to politely ask you to provide some more insight to terminology "Primary Assert/Deassert, Secondary Assert/Deassert". I do not follow Figure 306. TDD Frame Timing Illustration and the explanation is very brief. Is the purpose to allow two different lengths of Rx/Tx time slots? Meaning, only Primary Assert/Deassert could be used?
Thank you and Regards,
Jakub