ADRV9002 Full Rate DPD Support

Hello,

My customer has come to me with a question on the sample rate of the DPD on the ADRV9002. When he tries to select a sample rate greater than 30.72MHz i.e 61.44MHz the TES GUI (V.015 ). Is there a configuration issue that limits the sample rate to 30.72MHz? 

Would this be considered as a custom setup that would be supported on TES GUI V0.16? I believe that V0.16 works on rev C silicon only. Is that correct? If not, will there be support for 61.44MHz in the future

Can you advise?

Thanks,

Anita

Parents Reply Children
No Data