ADRV9002 and Keysight 89601 VSA

The ADRV9009 TES outputs captured received data in the Keysight 89601 VSA format.

For example, the file contains the correct header information and it has the I/Q data in the correct format:

InputZoom    TRUE
InputCenter    1000000000
InputRange    1.0
InputRefImped    50.0
XStart    0.0
XDelta    4.16666667e-9
XDomain    2
XUnit    Sec
YUnit    V
FreqValidMax    1015000000
FreqValidMin    985000000
Y

I1 <tab> Q1

I2 <tab> Q2

I3 <tab> Q3

etc...

Can the ADRV9002 TES output the IQ data in the same format?

It seems to output the I and Q  it in this format instead:

I1

Q1

I2

Q2

I3

Q3

etc...

Parents Reply Children
No Data