Question on how to generate C code using ADRV9002 TES without EVB

My customer is developing a board with ADRV9002.

However, it seems that Demo Mode is not supported in the TES App for ADRV9002.

I don't have an EVB, but can I generate C code in TES demo mode?

please answer about my question.

  • +1
    •  Analog Employees 
    on Apr 26, 2021 8:53 AM

    Hello Sewon,

    There is an "offline" mode for the TES package which can be used to generate sample code:

    1. Enter the Windows Command terminal (press Win + R, type 'cmd', press Enter), and navigate to the directory where TES is stored.
    2. Type exactly this: "Argo.Navis.exe" --offline

    At this point TES will launch. Treat this GUI as if you were connecting to a device normally. Press the Connect button, program the part as normal, then generate your sample code. Bear in mind some parts of the generated code may need to be changed, given that the APIs were never called on a real device. Before deploying your code to your platform be sure to give it a thorough inspection.

    Let me know if there's any further questions!

    Best Regards,
    Oisín.

  • 0
    •  Analog Employees 
    on Jun 25, 2021 12:55 AM in reply to OWatkins

    Still works with latest 0.16 release.  A little easier to read using a monospaced font;

       "Argo.Navis.exe" --offline

  • 0
    •  Analog Employees 
    on Jun 25, 2021 8:03 AM in reply to chucks

    Thanks for providing that, definitely a lot easier to read.

    v0.16 also comes with a feature within TES to run in offline mode, simply start TES normally and press the "Use Demo Mode" button.

    Best Regards,
    Oisin.