TES Connection fails with ADRV9002 evaluation card + ZCU102.

[Hardware]
ZCU102 : Revision D2 PROD
ADRV9002NP/W1/PCBZ : Silicon Revision C0 (Clock switch is set to an on-board).

[Situation]
Ping to 192.168.1.10 is ok.
But TES Connection fails.

I have rebuilt the SD image by following steps 1 to 4 of "a) SD card image (SDK 13 or later)" in the following URL.
ez.analog.com/.../a-sd-card-image-sdk-13-or-higher

However, the situation where the TES connection fails is unchanged.
Also, changing the clock setting does not change the situation.

I'm attaching the boot log so please point out any problems.

boot.log
Xilinx Zynq MP First Stage Boot Loader 
Release 2019.2   Jan 24 2021  -  13:17:24
NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE:  BL31: Secure code at 0x0
NOTICE:  BL31: Non secure code at 0x8000000
NOTICE:  BL31: v1.4(release):1db0406-dirty
NOTICE:  BL31: Built : 13:28:10, Jan 24 2021
PMUFW:	v1.1


U-Boot 2018.01 (Jan 24 2021 - 13:25:30 -0500) Xilinx ZynqMP ZCU102 rev1.0

I2C:   ready
DRAM:  4 GiB
EL Level:	EL2
Chip ID:	zu9eg
MMC:   sdhci@ff170000: 0 (SD)
*** Warning - bad CRC, using default environment

In:    serial@ff000000
Out:   serial@ff000000
Err:   serial@ff000000
Bootmode: LVL_SHFT_SD_MODE1
Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

Warning: ethernet@ff0e0000 using MAC address from ROM
eth0: ethernet@ff0e0000
Hit any key to stop autoboot:  2  1  0 
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 3
OEM: 5344
Name: SB16G 
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.8 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uEnv.txt
188 bytes read in 9 ms (19.5 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
## Error: Can't overwrite "ethaddr"
himport_r: can't insert "ethaddr=00:0a:35:00:01:22" into hash table
reading system.dtb
37339 bytes read in 17 ms (2.1 MiB/s)
reading Image
16116224 bytes read in 1053 ms (14.6 MiB/s)
## Flattened Device Tree blob at 04000000
   Booting using the fdt blob at 0x4000000
   Loading Device Tree to 000000000fff3000, end 000000000ffff1da ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.0 (rkutty@rkutty-lx01.adsdesign.analog.com) (gcc version 8.2.0 (GCC)) #1 SMP Sun Jan 24 14:11:29 EST 2021
[    0.000000] Boot CPU: AArch64 Processor [410fd034]
[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] random: fast init done
[    0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff67000 s45080 r8192 d32744 u86016
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
[    0.000000] Kernel command line: console=ttyPS0,115200 clk_ignore_unused root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait uio_pdrv_genirq.of_id=generic-uio ip=192.168.1.10 root=/dev/mmcblk0p2 rw rootwait
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff]
[    0.000000] Memory: 3784120K/4194304K available (9468K kernel code, 634K rwdata, 5108K rodata, 512K init, 2152K bss, 148040K reserved, 262144K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
[    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
[    0.000000]       .text : 0xffffff8008080000 - 0xffffff80089c0000   (  9472 KB)
[    0.000000]     .rodata : 0xffffff80089c0000 - 0xffffff8008ec0000   (  5120 KB)
[    0.000000]       .init : 0xffffff8008ec0000 - 0xffffff8008f40000   (   512 KB)
[    0.000000]       .data : 0xffffff8008f40000 - 0xffffff8008fdea00   (   635 KB)
[    0.000000]        .bss : 0xffffff8008fdea00 - 0xffffff80091f8a68   (  2153 KB)
[    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
[    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
[    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
[    0.000000]               0xffffffbf00000000 - 0xffffffbf1dc00000   (   476 MB actual)
[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc880000000   ( 34816 MB)
[    0.000000] Hierarchical RCU implementation.
[    0.000000] 	RCU event tracing is enabled.
[    0.000000] 	RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns
[    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
[    0.000315] Console: colour dummy device 80x25
[    0.000334] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
[    0.000342] pid_max: default: 32768 minimum: 301
[    0.000441] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.000455] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.001009] ASID allocator initialised with 65536 entries
[    0.001056] Hierarchical SRCU implementation.
[    0.001402] EFI services will not be available.
[    0.001448] zynqmp_plat_init Platform Management API v1.1
[    0.001453] zynqmp_plat_init Trustzone version v1.0
[    0.001548] smp: Bringing up secondary CPUs ...
[    0.001787] Detected VIPT I-cache on CPU1
[    0.001815] CPU1: Booted secondary processor [410fd034]
[    0.002083] Detected VIPT I-cache on CPU2
[    0.002101] CPU2: Booted secondary processor [410fd034]
[    0.002357] Detected VIPT I-cache on CPU3
[    0.002375] CPU3: Booted secondary processor [410fd034]
[    0.002415] smp: Brought up 1 node, 4 CPUs
[    0.002429] SMP: Total of 4 processors activated.
[    0.002435] CPU features: detected feature: 32-bit EL0 Support
[    0.002442] CPU: All CPU(s) started at EL2
[    0.002455] alternatives: patching kernel code
[    0.003174] devtmpfs: initialized
[    0.008028] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.008043] futex hash table entries: 1024 (order: 5, 131072 bytes)
[    0.013444] xor: measuring software checksum speed
[    0.052009]    8regs     :  2375.000 MB/sec
[    0.092037]    8regs_prefetch:  2052.000 MB/sec
[    0.132066]    32regs    :  2724.000 MB/sec
[    0.172095]    32regs_prefetch:  2308.000 MB/sec
[    0.172099] xor: using function: 32regs (2724.000 MB/sec)
[    0.172161] pinctrl core: initialized pinctrl subsystem
[    0.172663] NET: Registered protocol family 16
[    0.173533] cpuidle: using governor menu
[    0.174200] vdso: 2 pages (1 code @ ffffff80089c6000, 1 data @ ffffff8008f44000)
[    0.174210] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.174665] DMA: preallocated 256 KiB pool for atomic allocations
[    0.206659] zynqmp-pinctrl pinctrl: zynqmp pinctrl initialized
[    0.207456] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
[    0.208031] ARM CCI_400_r1 PMU driver probed
[    0.217832] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.284348] raid6: int64x1  gen()   453 MB/s
[    0.352300] raid6: int64x1  xor()   437 MB/s
[    0.420380] raid6: int64x2  gen()   676 MB/s
[    0.488381] raid6: int64x2  xor()   586 MB/s
[    0.556444] raid6: int64x4  gen()   972 MB/s
[    0.624484] raid6: int64x4  xor()   726 MB/s
[    0.692504] raid6: int64x8  gen()  1157 MB/s
[    0.760563] raid6: int64x8  xor()   745 MB/s
[    0.828670] raid6: neonx1   gen()   736 MB/s
[    0.896649] raid6: neonx1   xor()   853 MB/s
[    0.964707] raid6: neonx2   gen()  1126 MB/s
[    1.032753] raid6: neonx2   xor()  1144 MB/s
[    1.100826] raid6: neonx4   gen()  1506 MB/s
[    1.168872] raid6: neonx4   xor()  1395 MB/s
[    1.236911] raid6: neonx8   gen()  1540 MB/s
[    1.304953] raid6: neonx8   xor()  1451 MB/s
[    1.304957] raid6: using algorithm neonx8 gen() 1540 MB/s
[    1.304961] raid6: .... xor() 1451 MB/s, rmw enabled
[    1.304965] raid6: using neon recovery algorithm
[    1.306273] SCSI subsystem initialized
[    1.306418] usbcore: registered new interface driver usbfs
[    1.306446] usbcore: registered new interface driver hub
[    1.306480] usbcore: registered new device driver usb
[    1.306536] media: Linux media interface: v0.10
[    1.306558] Linux video capture interface: v2.00
[    1.306594] pps_core: LinuxPPS API ver. 1 registered
[    1.306598] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    1.306612] PTP clock support registered
[    1.306634] EDAC MC: Ver: 3.0.0
[    1.307163] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.
[    1.307307] FPGA manager framework
[    1.307410] fpga-region fpga-full: FPGA Region probed
[    1.307494] Advanced Linux Sound Architecture Driver Initialized.
[    1.307729] Bluetooth: Core ver 2.22
[    1.307755] NET: Registered protocol family 31
[    1.307759] Bluetooth: HCI device and connection manager initialized
[    1.307766] Bluetooth: HCI socket layer initialized
[    1.307772] Bluetooth: L2CAP socket layer initialized
[    1.307786] Bluetooth: SCO socket layer initialized
[    1.308402] clocksource: Switched to clocksource arch_sys_counter
[    1.308469] VFS: Disk quotas dquot_6.6.0
[    1.308507] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.312313] NET: Registered protocol family 2
[    1.312601] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[    1.312805] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[    1.313183] TCP: Hash tables configured (established 32768 bind 32768)
[    1.313247] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[    1.313320] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[    1.313466] NET: Registered protocol family 1
[    1.313714] RPC: Registered named UNIX socket transport module.
[    1.313718] RPC: Registered udp transport module.
[    1.313722] RPC: Registered tcp transport module.
[    1.313726] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.314256] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    1.314396] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.314991] audit: initializing netlink subsys (disabled)
[    1.315134] audit: type=2000 audit(1.304:1): state=initialized audit_enabled=0 res=1
[    1.315520] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    1.316186] NFS: Registering the id_resolver key type
[    1.316201] Key type id_resolver registered
[    1.316205] Key type id_legacy registered
[    1.316213] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.316230] jffs2: version 2.2. (NAND) (SUMMARY)  c 2001-2006 Red Hat, Inc.
[    1.339923] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    1.339931] io scheduler noop registered
[    1.339935] io scheduler deadline registered
[    1.339951] io scheduler cfq registered (default)
[    1.339956] io scheduler mq-deadline registered
[    1.339960] io scheduler kyber registered
[    1.340554] nwl-pcie fd0e0000.pcie: Link is DOWN
[    1.340594] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:
[    1.340610] OF: PCI:   MEM 0xe0000000..0xefffffff -> 0xe0000000
[    1.340618] OF: PCI:   MEM 0x600000000..0x7ffffffff -> 0x600000000
[    1.340738] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[    1.340747] pci_bus 0000:00: root bus resource [bus 00-ff]
[    1.340753] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[    1.340759] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[    1.341006] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
[    1.341759] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    1.342139] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[    1.342292] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[    1.342440] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[    1.342591] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[    1.342740] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[    1.342891] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[    1.343048] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[    1.343199] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[    1.367685] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    1.370644] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    1.374491] brd: module loaded
[    1.377725] loop: module loaded
[    1.378482] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517
[    1.378630] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.379401] m25p80 spi0.0: found n25q512a, expected m25p80
[    1.379628] m25p80 spi0.0: n25q512a (131072 Kbytes)
[    1.379648] 4 ofpart partitions found on MTD device spi0.0
[    1.379652] Creating 4 MTD partitions on "spi0.0":
[    1.379661] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    1.380061] 0x000000100000-0x000000600000 : "qspi-linux"
[    1.380444] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    1.380812] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[    1.381987] libphy: Fixed MDIO Bus: probed
[    1.382905] tun: Universal TUN/TAP device driver, 1.6
[    1.383035] CAN device driver interface
[    1.385105] macb ff0e0000.ethernet: Not enabling partial store and forward
[    1.385473] libphy: MACB_mii_bus: probed
[    1.387101] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 23 (00:0a:35:03:2b:68)
[    1.387109] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
[    1.387617] usbcore: registered new interface driver asix
[    1.387663] usbcore: registered new interface driver ax88179_178a
[    1.387687] usbcore: registered new interface driver cdc_ether
[    1.387712] usbcore: registered new interface driver net1080
[    1.387735] usbcore: registered new interface driver cdc_subset
[    1.387758] usbcore: registered new interface driver zaurus
[    1.387791] usbcore: registered new interface driver cdc_ncm
[    1.388331] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    1.389649] usbcore: registered new interface driver uas
[    1.389681] usbcore: registered new interface driver usb-storage
[    1.390132] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[    1.390176] i2c /dev entries driver
[    1.391158] IR NEC protocol handler initialized
[    1.391163] IR RC5(x/sz) protocol handler initialized
[    1.391167] IR RC6 protocol handler initialized
[    1.391170] IR JVC protocol handler initialized
[    1.391173] IR Sony protocol handler initialized
[    1.391177] IR SANYO protocol handler initialized
[    1.391180] IR Sharp protocol handler initialized
[    1.391184] IR MCE Keyboard/mouse protocol handler initialized
[    1.391187] IR XMP protocol handler initialized
[    1.392101] usbcore: registered new interface driver uvcvideo
[    1.392105] USB Video Class driver (1.1.1)
[    1.392680] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff800926d000 with timeout 10s
[    1.392854] Bluetooth: HCI UART driver ver 2.3
[    1.392860] Bluetooth: HCI UART protocol H4 registered
[    1.392864] Bluetooth: HCI UART protocol BCSP registered
[    1.392885] Bluetooth: HCI UART protocol LL registered
[    1.392890] Bluetooth: HCI UART protocol ATH3K registered
[    1.392894] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    1.392930] Bluetooth: HCI UART protocol Intel registered
[    1.392935] Bluetooth: HCI UART protocol QCA registered
[    1.392967] usbcore: registered new interface driver bcm203x
[    1.392994] usbcore: registered new interface driver bpa10x
[    1.393025] usbcore: registered new interface driver bfusb
[    1.393054] usbcore: registered new interface driver btusb
[    1.393058] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    1.393101] usbcore: registered new interface driver ath3k
[    1.393227] EDAC MC: ECC not enabled
[    1.393373] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    1.394236] sdhci: Secure Digital Host Controller Interface driver
[    1.394240] sdhci: Copyright(c) Pierre Ossman
[    1.394244] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.395355] ledtrig-cpu: registered to indicate activity on CPUs
[    1.395485] usbcore: registered new interface driver usbhid
[    1.395489] usbhid: USB HID core driver
[    1.397244] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    1.397900] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    1.398203] Netfilter messages via NETLINK v0.30.
[    1.398318] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.398432] Initializing XFRM netlink socket
[    1.398486] NET: Registered protocol family 10
[    1.398865] Segment Routing with IPv6
[    1.398903] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    1.399018] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.399312] NET: Registered protocol family 17
[    1.399325] NET: Registered protocol family 15
[    1.399339] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    1.399345] Ebtables v2.0 registered
[    1.399655] can: controller area network core (rev 20170425 abi 9)
[    1.399683] NET: Registered protocol family 29
[    1.399694] can: raw protocol (rev 20170425)
[    1.399699] can: broadcast manager protocol (rev 20170425 t)
[    1.399705] can: netlink gateway (rev 20170425) max_hops=1
[    1.399819] Bluetooth: RFCOMM TTY layer initialized
[    1.399827] Bluetooth: RFCOMM socket layer initialized
[    1.399837] Bluetooth: RFCOMM ver 1.11
[    1.399844] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    1.399847] Bluetooth: BNEP filters: protocol multicast
[    1.399854] Bluetooth: BNEP socket layer initialized
[    1.399858] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    1.399864] Bluetooth: HIDP socket layer initialized
[    1.399965] 9pnet: Installing 9P2000 support
[    1.399981] Key type dns_resolver registered
[    1.400562] registered taskstats version 1
[    1.400922] Btrfs loaded, crc32c=crc32c-generic
[    1.406101] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 39, base_baud = 6249999) is a xuartps
[    2.935712] console [ttyPS0] enabled
[    2.939930] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 40, base_baud = 6249999) is a xuartps
[    2.950583] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
[    2.958696] PLL: shutdown
[    2.961380] PLL: shutdown
[    2.964300] PLL: enable
[    2.966808] PLL: shutdown
[    2.970744] PLL: enable
[    2.973220] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[    2.983801] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    2.991756] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    3.000000] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.012341] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.024924] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[    3.035007] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.041905] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.048431] [drm] No driver support for vblank timestamp query.
[    3.054391] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008a77628)
[    3.098352] PLL: enable
[    3.195828] Console: switching to colour frame buffer device 128x48
[    3.217763] zynqmp-display fd4a0000.zynqmp-display: fb0:  frame buffer device
[    3.225048] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[    3.233074] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[    3.242082] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
[    3.249887] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
[    3.258773] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst 
[    3.269066] scsi host0: ahci-ceva
[    3.272469] scsi host1: ahci-ceva
[    3.275785] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37
[    3.283617] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37
[    3.293349] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
[    3.301362] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    3.306777] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    3.314648] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010
[    3.323288] xhci-hcd xhci-hcd.0.auto: irq 45, io mem 0xfe200000
[    3.329270] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    3.335984] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    3.343183] usb usb1: Product: xHCI Host Controller
[    3.348043] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd
[    3.353425] usb usb1: SerialNumber: xhci-hcd.0.auto
[    3.358560] hub 1-0:1.0: USB hub found
[    3.362249] hub 1-0:1.0: 1 port detected
[    3.366308] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    3.371715] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    3.379388] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    3.387488] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[    3.394192] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    3.401394] usb usb2: Product: xHCI Host Controller
[    3.406255] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd
[    3.411637] usb usb2: SerialNumber: xhci-hcd.0.auto
[    3.416726] hub 2-0:1.0: USB hub found
[    3.420410] hub 2-0:1.0: 1 port detected
[    3.425379] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
[    3.435486] GPIO line 322 (sel0) hogged as output/low
[    3.440789] GPIO line 323 (sel1) hogged as output/high
[    3.446177] GPIO line 324 (sel2) hogged as output/high
[    3.451565] GPIO line 325 (sel3) hogged as output/high
[    3.456713] pca953x 0-0020: interrupt support not compiled in
[    3.462470] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
[    3.472377] pca953x 0-0021: interrupt support not compiled in
[    3.478827] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.485518] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.492208] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.498899] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.505592] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.512278] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.518965] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.525663] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.532350] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.539043] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.545347] i2c i2c-0: Added multiplexed i2c bus 3
[    3.550692] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
[    3.557387] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.564077] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.570764] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.577457] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.584152] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.590842] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.597536] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    3.603835] i2c i2c-0: Added multiplexed i2c bus 4
[    3.606608] ata2: SATA link down (SStatus 0 SControl 330)
[    3.610591] ata1: SATA link down (SStatus 0 SControl 330)
[    3.660335] i2c i2c-0: Added multiplexed i2c bus 5
[    3.665159] i2c i2c-0: Added multiplexed i2c bus 6
[    3.669873] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
[    3.677183] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 25
[    3.684742] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
[    3.691390] i2c i2c-1: Added multiplexed i2c bus 7
[    3.696321] i2c i2c-1: Added multiplexed i2c bus 8
[    3.703034] si570 9-005d: registered, current frequency 300000000 Hz
[    3.709336] i2c i2c-1: Added multiplexed i2c bus 9
[    3.715308] si570 10-005d: clock registration failed
[    3.720251] si570: probe of 10-005d failed with error -17
[    3.725595] i2c i2c-1: Added multiplexed i2c bus 10
[    3.730613] i2c i2c-1: Added multiplexed i2c bus 11
[    3.735531] i2c i2c-1: Added multiplexed i2c bus 12
[    3.740442] i2c i2c-1: Added multiplexed i2c bus 13
[    3.745350] i2c i2c-1: Added multiplexed i2c bus 14
[    3.750144] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
[    3.758315] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[    3.764960] i2c i2c-1: Added multiplexed i2c bus 15
[    3.769912] i2c i2c-1: Added multiplexed i2c bus 16
[    3.774825] i2c i2c-1: Added multiplexed i2c bus 17
[    3.779737] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@19
[    3.788272] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@19
[    3.797210] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@30
[    3.805802] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@30
[    3.814747] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@35
[    3.823337] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@35
[    3.832279] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@36
[    3.840875] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@36
[    3.849816] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@51
[    3.858409] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@51
[    3.867355] i2c i2c-1: Added multiplexed i2c bus 18
[    3.872329] i2c i2c-1: Added multiplexed i2c bus 19
[    3.877247] i2c i2c-1: Added multiplexed i2c bus 20
[    3.882157] i2c i2c-1: Added multiplexed i2c bus 21
[    3.887070] i2c i2c-1: Added multiplexed i2c bus 22
[    3.891867] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
[    3.899437] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 26
[    3.952411] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit
[    3.967150] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    3.973965] rtc_zynqmp ffa60000.rtc: setting system clock to 2020-11-18 01:51:39 UTC (1605664299)
[    3.987276] pps pps0: new PPS source ptp0
[    3.991207] macb ff0e0000.ethernet: gem-ptp-timer ptp clock registered.
[    3.997845] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[    4.042074] mmc0: new high speed SDHC card at address aaaa
[    4.047662] mmcblk0: mmc0:aaaa SB16G 14.8 GiB 
[    4.055937]  mmcblk0: p1 p2
[    4.996684] macb ff0e0000.ethernet eth0: link up (1000/Full)
[    5.004427] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[    5.024411] IP-Config: Guessing netmask 255.255.255.0
[    5.029379] IP-Config: Complete:
[    5.032597]      device=eth0, hwaddr=00:0a:35:03:2b:68, ipaddr=192.168.1.10, mask=255.255.255.0, gw=255.255.255.255
[    5.043006]      host=192.168.1.10, domain=, nis-domain=(none)
[    5.048832]      bootserver=255.255.255.255, rootserver=255.255.255.255, rootpath=
[    5.056441] clk: Not disabling unused clocks
[    5.060881] ALSA device list:
[    5.063757]   #0: DisplayPort monitor
[    5.392854] EXT4-fs (mmcblk0p2): recovery complete
[    5.398353] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    5.406395] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    5.414804] devtmpfs: mounted
[    5.417803] Freeing unused kernel memory: 512K

Welcome to Ubuntu 15.04!

Cannot add dependency job for unit org.freedesktop.resolve1.busname, ignoring: Unit org.freedesktop.resolve1.busname failed to load: No such file or directory.
Cannot add dependency job for unit display-manager.service, ignoring: Unit display-manager.service failed to load: No such file or directory.
[  OK  ] Reached target Remote File Systems (Pre).
[  OK  ] Created slice Root Slice.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Reached target Swap.
[  OK  ] Created slice System Slice.
[  OK  ] Reached target Slices.
[  OK  ] Created slice system-getty.slice.
[  OK  ] Created slice system-serial\x2dgetty.slice.
[  OK  ] Listening on Delayed Shutdown Socket.
         Starting Increase datagram queue length...
[  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
[  OK  ] Listening on udev Kernel Socket.
[  OK  ] Reached target Encrypted Volumes.
[  OK  ] Listening on Journal Socket (/dev/log).
[  OK  ] Reached target Paths.
[  OK  ] Listening on Journal Socket.
         Mounting POSIX Message Queue File System...
         Mounting Huge Pages File System...
         Starting Load Kernel Modules...
[  OK  ] Started Read required files in advance.
         Starting Read required files in advance...
         Mounting Temporary Directory...
[  OK  ] Started Boot Process Profiler.
         Starting Boot Process Profiler...
         Starting Create Static Device Nodes in /dev...
         Mounting Debug File System...
         Starting Remount Root and Kernel File Systems...
[  OK  ] Listening on networkd rtnetlink socket.
[  OK  ] Listening on udev Control Socket.
         Starting udev Coldplug all Devices...
[  OK  ] Listening on Journal Audit Socket.
         Starting Nameserver information manager...
[  OK  ] Started Remount Root and Kernel File Systems.
         Starting Load/Save Random Seed...
systemd-bootchart.service failed.
[  OK  ] Started Load Kernel Modules.
         Mounting Configuration File System...
         Starting Apply Kernel Variables...
[  OK  ] Mounted Debug File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted Configuration File System.
[  OK  ] Mounted Temporary Directory.
[  OK  ] Started Increase datagram queue length.
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started Nameserver information manager.
[  OK  ] Started Create Static Device Nodes in /dev.
ureadahead.service failed.
[  OK  ] Started udev Coldplug all Devices.
         Starting udev Kernel Device Manager...
[  OK  ] Reached target Local File Systems (Pre).
[  OK  ] Listening on Syslog Socket.
         Starting Journal Service...
[  OK  ] Reached target Local File Systems.
         Starting Wait for all "auto" /etc/n... up for network-online.target...
         Starting LSB: Raise network interfaces....
[  OK  ] Reached target Remote File Systems.
[  OK  ] Started Wait for all "auto" /etc/ne...be up for network-online.target.
[  OK  ] Started udev Kernel Device Manager.
         Starting Copy rules generated while the root was ro...
[  OK  ] Started Journal Service.
         Starting Flush Journal to Persistent Storage...
[  OK  ] Started Copy rules generated while the root was ro.
[  OK  ] Started Flush Journal to Persistent Storage.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Create Volatile Files and Directories.
[  OK  ] Found device /dev/ttyPS0.
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Reached target Sound Card.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Created slice system-ifup.slice.
[  OK  ] Started ifup for sit0.
         Starting ifup for sit0...
[  OK  ] Started ifup for eth1.
         Starting ifup for eth1...
[  OK  ] Started ifup for can0.
         Starting ifup for can0...
[*     ] A start job is running for LSB: Rai...work interfaces. (6s / no limit)[**    ] A start job is running for LSB: Rai...work interfaces. (6s / no limit)[***   ] A start job is running for LSB: Rai...work interfaces. (7s / no limit)[ ***  ] A start job is running for LSB: Rai...work interfaces. (8s / no limit)[  *** ] A start job is running for LSB: Rai...work interfaces. (8s / no limit)[   ***] A start job is running for LSB: Rai...work interfaces. (9s / no limit)[    **] A start job is running for LSB: Rai...work interfaces. (9s / no limit)[     *] A start job is running for LSB: Rai...ork interfaces. (10s / no limit)[    **] A start job is running for LSB: Rai...ork interfaces. (10s / no limit)[   ***] A start job is running for LSB: Rai...ork interfaces. (11s / no limit)[  *** ] A start job is running for LSB: Rai...ork interfaces. (11s / no limit)[ ***  ] A start job is running for LSB: Rai...ork interfaces. (12s / no limit)[***   ] A start job is running for LSB: Rai...ork interfaces. (12s / no limit)[**    ] A start job is running for LSB: Rai...ork interfaces. (13s / no limit)[*     ] A start job is running for LSB: Rai...ork interfaces. (13s / no limit)[**    ] A start job is running for LSB: Rai...ork interfaces. (14s / no limit)[***   ] A start job is running for LSB: Rai...ork interfaces. (14s / no limit)[ ***  ] A start job is running for LSB: Rai...ork interfaces. (15s / no limit)[  *** ] A start job is running for LSB: Rai...ork interfaces. (15s / no limit)[   ***] A start job is running for LSB: Rai...ork interfaces. (16s / no limit)[    **] A start job is running for LSB: Rai...ork interfaces. (16s / no limit)[     *] A start job is running for LSB: Rai...ork interfaces. (17s / no limit)[  OK  ] Started LSB: Raise network interfaces..
[  OK  ] Reached target System Initialization.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Listening on OpenBSD Secure Shell server socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
         Starting Login Service...
         Starting LSB: Load kernel modules needed to enable cpufreq scaling...
         Starting LSB: Set the CPU Frequency Scaling governor to "ondemand"...
         Starting LSB: Xen daemons...
[  OK  ] Reached target Containers.
         Starting Initialize hardware monitoring sensors...
         Starting Network Manager...
         Starting WPA supplicant...
         Starting Provide limited super user privileges to specific users...
[  OK  ] Started Regular background program processing daemon.
         Starting Regular background program processing daemon...
         Starting System Logging Service...
         Starting LSB: Platform initscript...
         Starting Permit User Sessions...
         Starting D-Bus System Message Bus...
[  OK  ] Reached target Timers.
[  OK  ] Started LSB: Load kernel modules needed to enable cpufreq scaling.
[  OK  ] Started LSB: Set the CPU Frequency Scaling governor to "ondemand".
[  OK  ] Started LSB: Xen daemons.
[  OK  ] Started Provide limited super user privileges to specific users.
[  OK  ] Started Permit User Sessions.
Running Platform Init
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Started Initialize hardware monitoring sensors.
[  OK  ] Started System Logging Service.
[  OK  ] Started WPA supplicant.
[  OK  ] Started Login Service.
         Starting Network Service...
         Starting LSB: Start/stop secondary xen domains...
         Starting LSB: set CPUFreq kernel parameters...
[  OK  ] Started Network Service.
[  OK  ] Started LSB: Start/stop secondary xen domains.
[  OK  ] Started LSB: set CPUFreq kernel parameters.
         Starting Authenticate and Authorize Users to Run Privileged Tasks...
         Starting Network Name Resolution...
[  OK  ] Started Network Name Resolution.
[  OK  ] Started Authenticate and Authorize Users to Run Privileged Tasks.
[  OK  ] Started Network Manager.
         Starting Network Manager Wait Online...
[  OK  ] Reached target Network.
         Starting /etc/rc.local Compatibility...
[  OK  ] Started Network Manager Wait Online.
[  OK  ] Stopped OpenBSD Secure Shell server.
[  OK  ] Started OpenBSD Secure Shell server.
         Starting OpenBSD Secure Shell server...
[  OK  ] Reached target Network is Online.
         Starting LSB: start Samba daemons for the AD DC...
         Starting LSB: start Samba NetBIOS nameserver (nmbd)...
[  OK  ] Stopped LSB: start Samba SMB/CIFS daemon (smbd).
         Starting LSB: start Samba SMB/CIFS daemon (smbd)...
[  OK  ] Closed OpenBSD Secure Shell server socket.
[  OK  ] Stopped OpenBSD Secure Shell server.
[  OK  ] Started OpenBSD Secure Shell server.
         Starting OpenBSD Secure Shell server...
[  OK  ] Started LSB: start Samba daemons for the AD DC.
[  OK  ] Started LSB: start Samba NetBIOS nameserver (nmbd).
[  OK  ] Started LSB: start Samba SMB/CIFS daemon (smbd).
[  OK  ] Started /etc/rc.local Compatibility.
[  OK  ] Started Serial Getty on ttyPS0.
         Starting Serial Getty on ttyPS0...
[  OK  ] Started Getty on tty1.
         Starting Getty on tty1...
[  OK  ] Reached target Login Prompts.
[  OK  ] Started LSB: Platform initscript.
[  OK  ] Reached target Multi-User System.
[  OK  ] Reached target Graphical Interface.
         Starting Update UTMP about System Runlevel Ch
Ubuntu 15.04 linaro-developer ttyPS0

linaro-developer login: root (automatic login)

Last login: Wed Nov 18 00:15:20 UTC 2020 on ttyPS0
root@linaro-developer:~#