I am having problems retargeting the axi_adrv9001 ip.
I was able to successfully create the axi_adrv9001 ip for the zcu102 board.
I cannot seem to retarget this for the zcu106 board.
If I open this in the ip packager and change to the zcu106 board and try to repackage IP there are critical warnings.
Then when I try to add this to my block design, I cannot use it as the IP is locked and I cannot upgrade.
I have tried to add the ip without using the ip packager to change it and the IP is also locked.
So how do I retarget this IP to the zcu106 board or in the end, some custom board?
Thanks for the help