TES Connection failure with ADRV9002 evaluation card + ZCU102

Hello,

I have connection failure with ADRV9002 evaluation card + ZCU102.

Attached is error log.

 

I downloaded tools from following site:

www.analog.com/.../transceiver-evaluation-software.html

ADRV9001-SDK Evaluation Software (ZIP)

Download SD Card Image Making Software (zip)

 

I followed instructions bellow to make SD card for ZCU102.

ez.analog.com/.../a-sd-card-image-sdk-13-or-higher

 

SD card I made includes following files:

- System Volume Information (folder)

- adrv9001_zcu102_cmos.bin

- adrv9001_zcu102_lvds.bin

- BOOT.bin

- Image

- system.dtb

- uEnv.txt

 

Ping to 192.168.1.10 is ok.

No security software on laptop PC.

There exists Adrv9001Server_B0_39.0.7, however when I tried to start it manually,

segmentation fault occurred. (see attached cmd_log.txt)

Xilinx Zynq MP First Stage Boot Loader 
Release 2019.2   Oct 15 2020  -  09:25:42
NOTICE:  ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000
NOTICE:  BL31: Secure code at 0x0
NOTICE:  BL31: Non secure code at 0x8000000
NOTICE:  BL31: v1.4(release):2dd13f9-dirty
NOTICE:  BL31: Built : 09:34:41, Oct 15 2020
PMUFW:	v1.1


U-Boot 2018.01 (Oct 15 2020 - 09:31:18 -0400) Xilinx ZynqMP ZCU102 rev1.0

I2C:   ready
DRAM:  4 GiB
EL Level:	EL2
Chip ID:	zu9eg
MMC:   sdhci@ff170000: 0 (SD)
*** Warning - bad CRC, using default environment

In:    serial@ff000000
Out:   serial@ff000000
Err:   serial@ff000000
Bootmode: LVL_SHFT_SD_MODE1
Net:   ZYNQ GEM: ff0e0000, phyaddr c, interface rgmii-id

Warning: ethernet@ff0e0000 using MAC address from ROM
eth0: ethernet@ff0e0000
Hit any key to stop autoboot:  2  1  0 
switch to partitions #0, OK
mmc0 is current device
Device: sdhci@ff170000
Manufacturer ID: 2
OEM: 544d
Name: SA16G 
Tran Speed: 50000000
Rd Block Len: 512
SD version 3.0
High Capacity: Yes
Capacity: 14.5 GiB
Bus Width: 4-bit
Erase Group Size: 512 Bytes
reading uEnv.txt
172 bytes read in 9 ms (18.6 KiB/s)
Loaded environment from uEnv.txt
Importing environment from SD ...
## Error: Can't overwrite "ethaddr"
himport_r: can't insert "ethaddr=00:0a:35:00:01:22" into hash table
reading system.dtb
37251 bytes read in 17 ms (2.1 MiB/s)
reading Image
16116224 bytes read in 1055 ms (14.6 MiB/s)
## Flattened Device Tree blob at 04000000
   Booting using the fdt blob at 0x4000000
   Loading Device Tree to 000000000fff3000, end 000000000ffff182 ... OK

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 4.14.0 (rkutty@rkutty-lx01.adsdesign.analog.com) (gcc version 8.2.0 (GCC)) #1 SMP Thu Oct 15 10:23:16 EDT 2020
[    0.000000] Boot CPU: AArch64 Processor [410fd034]
[    0.000000] Machine model: ZynqMP ZCU102 Rev1.0
[    0.000000] efi: Getting EFI parameters from FDT:
[    0.000000] efi: UEFI not found.
[    0.000000] cma: Reserved 256 MiB at 0x0000000070000000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: MIGRATE_INFO_TYPE not supported.
[    0.000000] random: fast init done
[    0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff67000 s45080 r8192 d32744 u86016
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: enabling workaround for ARM erratum 845719
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1034240
[    0.000000] Kernel command line: console=ttyPS0,115200 clk_ignore_unused root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait uio_pdrv_genirq.of_id=generic-uio root=/dev/mmcblk0p2 rw rootwait
[    0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes)
[    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes)
[    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes)
[    0.000000] software IO TLB [mem 0x6bfff000-0x6ffff000] (64MB) mapped at [ffffffc06bfff000-ffffffc06fffefff]
[    0.000000] Memory: 3784120K/4194304K available (9468K kernel code, 634K rwdata, 5108K rodata, 512K init, 2152K bss, 148040K reserved, 262144K cma-reserved)
[    0.000000] Virtual kernel memory layout:
[    0.000000]     modules : 0xffffff8000000000 - 0xffffff8008000000   (   128 MB)
[    0.000000]     vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000   (   250 GB)
[    0.000000]       .text : 0xffffff8008080000 - 0xffffff80089c0000   (  9472 KB)
[    0.000000]     .rodata : 0xffffff80089c0000 - 0xffffff8008ec0000   (  5120 KB)
[    0.000000]       .init : 0xffffff8008ec0000 - 0xffffff8008f40000   (   512 KB)
[    0.000000]       .data : 0xffffff8008f40000 - 0xffffff8008fdea00   (   635 KB)
[    0.000000]        .bss : 0xffffff8008fdea00 - 0xffffff80091f8a68   (  2153 KB)
[    0.000000]     fixed   : 0xffffffbefe7fd000 - 0xffffffbefec00000   (  4108 KB)
[    0.000000]     PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000   (    16 MB)
[    0.000000]     vmemmap : 0xffffffbf00000000 - 0xffffffc000000000   (     4 GB maximum)
[    0.000000]               0xffffffbf00000000 - 0xffffffbf1dc00000   (   476 MB actual)
[    0.000000]     memory  : 0xffffffc000000000 - 0xffffffc880000000   ( 34816 MB)
[    0.000000] Hierarchical RCU implementation.
[    0.000000] 	RCU event tracing is enabled.
[    0.000000] 	RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4.
[    0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000
[    0.000000] GIC: Using split EOI/Deactivate mode
[    0.000000] arch_timer: cp15 timer(s) running at 99.99MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x170f8de2d3, max_idle_ns: 440795206112 ns
[    0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns
[    0.000316] Console: colour dummy device 80x25
[    0.000336] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.98 BogoMIPS (lpj=399960)
[    0.000344] pid_max: default: 32768 minimum: 301
[    0.000443] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.000457] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes)
[    0.001028] ASID allocator initialised with 65536 entries
[    0.001075] Hierarchical SRCU implementation.
[    0.001420] EFI services will not be available.
[    0.001465] zynqmp_plat_init Platform Management API v1.1
[    0.001471] zynqmp_plat_init Trustzone version v1.0
[    0.001566] smp: Bringing up secondary CPUs ...
[    0.001808] Detected VIPT I-cache on CPU1
[    0.001836] CPU1: Booted secondary processor [410fd034]
[    0.002106] Detected VIPT I-cache on CPU2
[    0.002124] CPU2: Booted secondary processor [410fd034]
[    0.002382] Detected VIPT I-cache on CPU3
[    0.002399] CPU3: Booted secondary processor [410fd034]
[    0.002440] smp: Brought up 1 node, 4 CPUs
[    0.002454] SMP: Total of 4 processors activated.
[    0.002459] CPU features: detected feature: 32-bit EL0 Support
[    0.002467] CPU: All CPU(s) started at EL2
[    0.002480] alternatives: patching kernel code
[    0.003210] devtmpfs: initialized
[    0.008052] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.008067] futex hash table entries: 1024 (order: 5, 131072 bytes)
[    0.013580] xor: measuring software checksum speed
[    0.052014]    8regs     :  2375.000 MB/sec
[    0.092042]    8regs_prefetch:  2052.000 MB/sec
[    0.132071]    32regs    :  2724.000 MB/sec
[    0.172099]    32regs_prefetch:  2308.000 MB/sec
[    0.172104] xor: using function: 32regs (2724.000 MB/sec)
[    0.172169] pinctrl core: initialized pinctrl subsystem
[    0.172699] NET: Registered protocol family 16
[    0.173558] cpuidle: using governor menu
[    0.174221] vdso: 2 pages (1 code @ ffffff80089c6000, 1 data @ ffffff8008f44000)
[    0.174231] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.174689] DMA: preallocated 256 KiB pool for atomic allocations
[    0.206770] zynqmp-pinctrl pinctrl: zynqmp pinctrl initialized
[    0.207574] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed
[    0.208155] ARM CCI_400_r1 PMU driver probed
[    0.218011] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[    0.284267] raid6: int64x1  gen()   452 MB/s
[    0.352337] raid6: int64x1  xor()   437 MB/s
[    0.420313] raid6: int64x2  gen()   675 MB/s
[    0.488389] raid6: int64x2  xor()   586 MB/s
[    0.556457] raid6: int64x4  gen()   973 MB/s
[    0.624489] raid6: int64x4  xor()   726 MB/s
[    0.692497] raid6: int64x8  gen()  1157 MB/s
[    0.760575] raid6: int64x8  xor()   747 MB/s
[    0.828586] raid6: neonx1   gen()   735 MB/s
[    0.896642] raid6: neonx1   xor()   853 MB/s
[    0.964684] raid6: neonx2   gen()  1126 MB/s
[    1.032740] raid6: neonx2   xor()  1145 MB/s
[    1.100773] raid6: neonx4   gen()  1506 MB/s
[    1.168806] raid6: neonx4   xor()  1395 MB/s
[    1.236889] raid6: neonx8   gen()  1540 MB/s
[    1.304897] raid6: neonx8   xor()  1451 MB/s
[    1.304901] raid6: using algorithm neonx8 gen() 1540 MB/s
[    1.304905] raid6: .... xor() 1451 MB/s, rmw enabled
[    1.304909] raid6: using neon recovery algorithm
[    1.306252] SCSI subsystem initialized
[    1.306403] usbcore: registered new interface driver usbfs
[    1.306436] usbcore: registered new interface driver hub
[    1.306473] usbcore: registered new device driver usb
[    1.306527] media: Linux media interface: v0.10
[    1.306549] Linux video capture interface: v2.00
[    1.306582] pps_core: LinuxPPS API ver. 1 registered
[    1.306586] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[    1.306599] PTP clock support registered
[    1.306620] EDAC MC: Ver: 3.0.0
[    1.306922] zynqmp-ipi ff9905c0.mailbox: Probed ZynqMP IPI Mailbox driver.
[    1.307060] FPGA manager framework
[    1.307155] fpga-region fpga-full: FPGA Region probed
[    1.307237] Advanced Linux Sound Architecture Driver Initialized.
[    1.307484] Bluetooth: Core ver 2.22
[    1.307511] NET: Registered protocol family 31
[    1.307515] Bluetooth: HCI device and connection manager initialized
[    1.307523] Bluetooth: HCI socket layer initialized
[    1.307529] Bluetooth: L2CAP socket layer initialized
[    1.307545] Bluetooth: SCO socket layer initialized
[    1.308169] clocksource: Switched to clocksource arch_sys_counter
[    1.308240] VFS: Disk quotas dquot_6.6.0
[    1.308282] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    1.312059] NET: Registered protocol family 2
[    1.312358] TCP established hash table entries: 32768 (order: 6, 262144 bytes)
[    1.312563] TCP bind hash table entries: 32768 (order: 7, 524288 bytes)
[    1.312972] TCP: Hash tables configured (established 32768 bind 32768)
[    1.313038] UDP hash table entries: 2048 (order: 4, 65536 bytes)
[    1.313111] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes)
[    1.313262] NET: Registered protocol family 1
[    1.313437] RPC: Registered named UNIX socket transport module.
[    1.313441] RPC: Registered udp transport module.
[    1.313445] RPC: Registered tcp transport module.
[    1.313448] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    1.313975] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[    1.314118] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[    1.314730] audit: initializing netlink subsys (disabled)
[    1.315049] audit: type=2000 audit(1.304:1): state=initialized audit_enabled=0 res=1
[    1.315114] workingset: timestamp_bits=62 max_order=20 bucket_order=0
[    1.315760] NFS: Registering the id_resolver key type
[    1.315776] Key type id_resolver registered
[    1.315779] Key type id_legacy registered
[    1.315788] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    1.315805] jffs2: version 2.2. (NAND) (SUMMARY)  c 2001-2006 Red Hat, Inc.
[    1.339497] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 246)
[    1.339506] io scheduler noop registered
[    1.339511] io scheduler deadline registered
[    1.339528] io scheduler cfq registered (default)
[    1.339532] io scheduler mq-deadline registered
[    1.339537] io scheduler kyber registered
[    1.340116] nwl-pcie fd0e0000.pcie: Link is DOWN
[    1.340155] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges:
[    1.340183] OF: PCI:   MEM 0xe0000000..0xefffffff -> 0xe0000000
[    1.340191] OF: PCI:   MEM 0x600000000..0x7ffffffff -> 0x600000000
[    1.340316] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00
[    1.340325] pci_bus 0000:00: root bus resource [bus 00-ff]
[    1.340332] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff]
[    1.340338] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref]
[    1.340593] pci 0000:00:00.0: PCI bridge to [bus 01-0c]
[    1.341380] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed
[    1.341768] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success
[    1.341922] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success
[    1.342077] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success
[    1.342230] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success
[    1.342384] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success
[    1.342543] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success
[    1.342701] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success
[    1.342856] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success
[    1.367209] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled
[    1.370144] cacheinfo: Unable to detect cache hierarchy for CPU 0
[    1.374159] brd: module loaded
[    1.377498] loop: module loaded
[    1.378260] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517
[    1.378405] mtdoops: mtd device (mtddev=name/number) must be supplied
[    1.379191] m25p80 spi0.0: found n25q512a, expected m25p80
[    1.379430] m25p80 spi0.0: n25q512a (131072 Kbytes)
[    1.379449] 4 ofpart partitions found on MTD device spi0.0
[    1.379454] Creating 4 MTD partitions on "spi0.0":
[    1.379461] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot"
[    1.379852] 0x000000100000-0x000000600000 : "qspi-linux"
[    1.380233] 0x000000600000-0x000000620000 : "qspi-device-tree"
[    1.380598] 0x000000620000-0x000000c00000 : "qspi-rootfs"
[    1.381762] libphy: Fixed MDIO Bus: probed
[    1.382687] tun: Universal TUN/TAP device driver, 1.6
[    1.382820] CAN device driver interface
[    1.384901] macb ff0e0000.ethernet: Not enabling partial store and forward
[    1.385268] libphy: MACB_mii_bus: probed
[    1.386894] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 23 (00:0a:35:05:60:38)
[    1.386902] TI DP83867 ff0e0000.ethernet-ffffffff:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.ethernet-ffffffff:0c, irq=POLL)
[    1.387413] usbcore: registered new interface driver asix
[    1.387455] usbcore: registered new interface driver ax88179_178a
[    1.387479] usbcore: registered new interface driver cdc_ether
[    1.387504] usbcore: registered new interface driver net1080
[    1.387530] usbcore: registered new interface driver cdc_subset
[    1.387555] usbcore: registered new interface driver zaurus
[    1.387589] usbcore: registered new interface driver cdc_ncm
[    1.388102] xilinx-axipmon ffa00000.perf-monitor: Probed Xilinx APM
[    1.389528] usbcore: registered new interface driver uas
[    1.389562] usbcore: registered new interface driver usb-storage
[    1.390031] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0
[    1.390077] i2c /dev entries driver
[    1.391073] IR NEC protocol handler initialized
[    1.391078] IR RC5(x/sz) protocol handler initialized
[    1.391082] IR RC6 protocol handler initialized
[    1.391085] IR JVC protocol handler initialized
[    1.391088] IR Sony protocol handler initialized
[    1.391092] IR SANYO protocol handler initialized
[    1.391095] IR Sharp protocol handler initialized
[    1.391099] IR MCE Keyboard/mouse protocol handler initialized
[    1.391102] IR XMP protocol handler initialized
[    1.392018] usbcore: registered new interface driver uvcvideo
[    1.392021] USB Video Class driver (1.1.1)
[    1.392580] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff800926d000 with timeout 10s
[    1.392737] Bluetooth: HCI UART driver ver 2.3
[    1.392744] Bluetooth: HCI UART protocol H4 registered
[    1.392748] Bluetooth: HCI UART protocol BCSP registered
[    1.392770] Bluetooth: HCI UART protocol LL registered
[    1.392775] Bluetooth: HCI UART protocol ATH3K registered
[    1.392779] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    1.392815] Bluetooth: HCI UART protocol Intel registered
[    1.392819] Bluetooth: HCI UART protocol QCA registered
[    1.392851] usbcore: registered new interface driver bcm203x
[    1.392881] usbcore: registered new interface driver bpa10x
[    1.392909] usbcore: registered new interface driver bfusb
[    1.392937] usbcore: registered new interface driver btusb
[    1.392942] Bluetooth: Generic Bluetooth SDIO driver ver 0.1
[    1.392985] usbcore: registered new interface driver ath3k
[    1.393095] EDAC MC: ECC not enabled
[    1.393267] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT)
[    1.394092] sdhci: Secure Digital Host Controller Interface driver
[    1.394096] sdhci: Copyright(c) Pierre Ossman
[    1.394099] sdhci-pltfm: SDHCI platform and OF driver helper
[    1.395251] ledtrig-cpu: registered to indicate activity on CPUs
[    1.395369] usbcore: registered new interface driver usbhid
[    1.395373] usbhid: USB HID core driver
[    1.397169] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered
[    1.397853] pktgen: Packet Generator for packet performance testing. Version: 2.75
[    1.398085] Netfilter messages via NETLINK v0.30.
[    1.398198] ip_tables: (C) 2000-2006 Netfilter Core Team
[    1.398325] Initializing XFRM netlink socket
[    1.398380] NET: Registered protocol family 10
[    1.398768] Segment Routing with IPv6
[    1.398807] ip6_tables: (C) 2000-2006 Netfilter Core Team
[    1.398919] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    1.399223] NET: Registered protocol family 17
[    1.399234] NET: Registered protocol family 15
[    1.399249] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this.
[    1.399254] Ebtables v2.0 registered
[    1.399332] can: controller area network core (rev 20170425 abi 9)
[    1.399360] NET: Registered protocol family 29
[    1.399371] can: raw protocol (rev 20170425)
[    1.399375] can: broadcast manager protocol (rev 20170425 t)
[    1.399382] can: netlink gateway (rev 20170425) max_hops=1
[    1.399574] Bluetooth: RFCOMM TTY layer initialized
[    1.399582] Bluetooth: RFCOMM socket layer initialized
[    1.399596] Bluetooth: RFCOMM ver 1.11
[    1.399604] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    1.399607] Bluetooth: BNEP filters: protocol multicast
[    1.399614] Bluetooth: BNEP socket layer initialized
[    1.399618] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    1.399623] Bluetooth: HIDP socket layer initialized
[    1.399719] 9pnet: Installing 9P2000 support
[    1.399735] Key type dns_resolver registered
[    1.400206] registered taskstats version 1
[    1.400509] Btrfs loaded, crc32c=crc32c-generic
[    1.405822] ff000000.serial: ttyPS0 at MMIO 0xff000000 (irq = 39, base_baud = 6249999) is a xuartps
[    2.934054] console [ttyPS0] enabled
[    2.938266] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 40, base_baud = 6249999) is a xuartps
[    2.948958] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes
[    2.957074] PLL: shutdown
[    2.959746] PLL: shutdown
[    2.962686] PLL: enable
[    2.965194] PLL: shutdown
[    2.969139] PLL: enable
[    2.971607] xilinx-dp-snd-codec fd4a0000.zynqmp-display:zynqmp_dp_snd_codec0: Xilinx DisplayPort Sound Codec probed
[    2.982204] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed
[    2.990161] xilinx-dp-snd-pcm zynqmp_dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed
[    2.998428] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.010772] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok
[    3.023356] xilinx-dp-snd-card fd4a0000.zynqmp-display:zynqmp_dp_snd_card: Xilinx DisplayPort Sound Card probed
[    3.033452] OF: graph: no port node found in /amba/zynqmp-display@fd4a0000
[    3.040363] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[    3.046894] [drm] No driver support for vblank timestamp query.
[    3.052857] xlnx-drm xlnx-drm.0: bound fd4a0000.zynqmp-display (ops 0xffffff8008a77628)
[    4.140185] [drm] Cannot find any crtc or sizes
[    4.144801] [drm] Initialized xlnx 1.0.0 20130509 for fd4a0000.zynqmp-display on minor 0
[    4.152821] zynqmp-display fd4a0000.zynqmp-display: ZynqMP DisplayPort Subsystem driver probed
[    4.161790] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes
[    4.169598] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode
[    4.178485] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst 
[    4.188801] scsi host0: ahci-ceva
[    4.192224] scsi host1: ahci-ceva
[    4.195542] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 37
[    4.203383] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 37
[    4.213036] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes
[    4.221012] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    4.226431] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1
[    4.234259] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x22010010
[    4.242901] xhci-hcd xhci-hcd.0.auto: irq 45, io mem 0xfe200000
[    4.248892] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[    4.255597] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    4.262799] usb usb1: Product: xHCI Host Controller
[    4.267659] usb usb1: Manufacturer: Linux 4.14.0 xhci-hcd
[    4.273041] usb usb1: SerialNumber: xhci-hcd.0.auto
[    4.278164] hub 1-0:1.0: USB hub found
[    4.281848] hub 1-0:1.0: 1 port detected
[    4.285907] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller
[    4.291313] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2
[    4.298994] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[    4.307089] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003
[    4.313790] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    4.320995] usb usb2: Product: xHCI Host Controller
[    4.325855] usb usb2: Manufacturer: Linux 4.14.0 xhci-hcd
[    4.331236] usb usb2: SerialNumber: xhci-hcd.0.auto
[    4.336326] hub 2-0:1.0: USB hub found
[    4.339997] hub 2-0:1.0: 1 port detected
[    4.345008] pca953x 0-0020: 0-0020 supply vcc not found, using dummy regulator
[    4.355123] GPIO line 322 (sel0) hogged as output/low
[    4.360431] GPIO line 323 (sel1) hogged as output/high
[    4.365820] GPIO line 324 (sel2) hogged as output/high
[    4.371208] GPIO line 325 (sel3) hogged as output/high
[    4.376366] pca953x 0-0020: interrupt support not compiled in
[    4.382120] pca953x 0-0021: 0-0021 supply vcc not found, using dummy regulator
[    4.392023] pca953x 0-0021: interrupt support not compiled in
[    4.398624] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.405325] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.412018] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.418708] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.425393] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.432081] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.438769] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.445459] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.452171] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.458863] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.465161] i2c i2c-0: Added multiplexed i2c bus 3
[    4.470505] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm)
[    4.477198] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.483884] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.490570] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.497263] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.503963] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.510647] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.517334] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm)
[    4.523633] i2c i2c-0: Added multiplexed i2c bus 4
[    4.526373] ata2: SATA link down (SStatus 0 SControl 330)
[    4.526396] ata1: SATA link down (SStatus 0 SControl 330)
[    4.580144] i2c i2c-0: Added multiplexed i2c bus 5
[    4.584970] i2c i2c-0: Added multiplexed i2c bus 6
[    4.589680] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544
[    4.596990] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 25
[    4.604558] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
[    4.611204] i2c i2c-1: Added multiplexed i2c bus 7
[    4.616132] i2c i2c-1: Added multiplexed i2c bus 8
[    4.622845] si570 9-005d: registered, current frequency 300000000 Hz
[    4.629145] i2c i2c-1: Added multiplexed i2c bus 9
[    4.635113] si570 10-005d: clock registration failed
[    4.640055] si570: probe of 10-005d failed with error -17
[    4.645392] i2c i2c-1: Added multiplexed i2c bus 10
[    4.650412] i2c i2c-1: Added multiplexed i2c bus 11
[    4.655323] i2c i2c-1: Added multiplexed i2c bus 12
[    4.660231] i2c i2c-1: Added multiplexed i2c bus 13
[    4.665145] i2c i2c-1: Added multiplexed i2c bus 14
[    4.669945] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548
[    4.677792] i2c i2c-1: Added multiplexed i2c bus 15
[    4.682710] i2c i2c-1: Added multiplexed i2c bus 16
[    4.687616] i2c i2c-1: Added multiplexed i2c bus 17
[    4.692520] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@19
[    4.701047] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@19
[    4.709986] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@30
[    4.718578] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@30
[    4.727520] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@35
[    4.736113] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@35
[    4.745058] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@36
[    4.753649] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@36
[    4.762590] i2c i2c-18: of_i2c: modalias failure on /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@51
[    4.771186] i2c i2c-18: Failed to create I2C device for /amba/i2c@ff030000/i2c-mux@75/i2c@3/dev@51
[    4.780131] i2c i2c-1: Added multiplexed i2c bus 18
[    4.785110] i2c i2c-1: Added multiplexed i2c bus 19
[    4.790017] i2c i2c-1: Added multiplexed i2c bus 20
[    4.794928] i2c i2c-1: Added multiplexed i2c bus 21
[    4.799844] i2c i2c-1: Added multiplexed i2c bus 22
[    4.804644] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548
[    4.812214] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 26
[    4.864179] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit
[    4.878939] input: gpio-keys as /devices/platform/gpio-keys/input/input0
[    4.885751] rtc_zynqmp ffa60000.rtc: setting system clock to 2021-01-10 05:44:06 UTC (1610257446)
[    4.894661] clk: Not disabling unused clocks
[    4.899091] ALSA device list:
[    4.901977]   #0: DisplayPort monitor
[    4.908203] Waiting for root device /dev/mmcblk0p2...
[    4.946135] mmc0: new high speed SDHC card at address 1234
[    4.951700] mmcblk0: mmc0:1234 SA16G 14.5 GiB 
[    4.957020]  mmcblk0: p1 p2
[    5.336184] [drm] Cannot find any crtc or sizes
[    8.736796] EXT4-fs (mmcblk0p2): recovery complete
[    8.743618] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[    8.751648] VFS: Mounted root (ext4 filesystem) on device 179:2.
[    8.758623] devtmpfs: mounted
[    8.761619] Freeing unused kernel memory: 512K

Welcome to Ubuntu 15.04!

Cannot add dependency job for unit org.freedesktop.resolve1.busname, ignoring: Unit org.freedesktop.resolve1.busname failed to load: No such file or directory.
Cannot add dependency job for unit display-manager.service, ignoring: Unit display-manager.service failed to load: No such file or directory.
[  OK  ] Created slice Root Slice.
[  OK  ] Listening on Journal Socket.
[  OK  ] Listening on udev Kernel Socket.
[  OK  ] Listening on networkd rtnetlink socket.
[  OK  ] Listening on Journal Audit Socket.
[  OK  ] Reached target Encrypted Volumes.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Listening on Journal Socket (/dev/log).
[  OK  ] Created slice System Slice.
         Mounting Huge Pages File System...
         Mounting Debug File System...
[  OK  ] Created slice system-getty.slice.
         Starting Nameserver information manager...
         Starting Load Kernel Modules...
         Mounting POSIX Message Queue File System...
         Starting Create Static Device Nodes in /dev...
         Mounting Temporary Directory...
[  OK  ] Reached target Slices.
         Starting Remount Root and Kernel File Systems...
[  OK  ] Listening on Delayed Shutdown Socket.
[  OK  ] Reached target Paths.
[  OK  ] Started Read required files in advance.
         Starting Read required files in advance...
         Starting Increase datagram queue length...
[  OK  ] Reached target Swap.
[  OK  ] Listening on udev Control Socket.
         Starting udev Coldplug all Devices...
[  OK  ] Created slice system-serial\x2dgetty.slice.
[  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
[  OK  ] Reached target Remote File Systems (Pre).
[  OK  ] Started Boot Process Profiler.
         Starting Boot Process Profiler...
[  OK  ] Started Remount Root and Kernel File Systems.
         Starting Load/Save Random Seed...
systemd-bootchart.service failed.
[  OK  ] Started Load/Save Random Seed.
[  OK  ] Started Load Kernel Modules.
[  OK  ] Mounted Debug File System.
[  OK  ] Mounted POSIX Message Queue File System.
[  OK  ] Mounted Huge Pages File System.
[  OK  ] Mounted Temporary Directory.
[  OK  ] Started Create Static Device Nodes in /dev.
[  OK  ] Started Increase datagram queue length.
[  OK  ] Started Nameserver information manager.
[  OK  ] Started udev Coldplug all Devices.
ureadahead.service failed.
[  OK  ] Listening on Syslog Socket.
         Starting Journal Service...
         Starting udev Kernel Device Manager...
[  OK  ] Reached target Local File Systems (Pre).
[  OK  ] Reached target Local File Systems.
         Starting Wait for all "auto" /etc/n... up for network-online.target...
[  OK  ] Reached target Remote File Systems.
         Mounting Configuration File System...
         Starting Apply Kernel Variables...
         Starting LSB: Raise network interfaces....
[  OK  ] Mounted Configuration File System.
[  OK  ] Started Wait for all "auto" /etc/ne...be up for network-online.target.
[  OK  ] Started Apply Kernel Variables.
[  OK  ] Started udev Kernel Device Manager.
         Starting Copy rules generated while the root was ro...
[  OK  ] Started Journal Service.
[  OK  ] Started Copy rules generated while the root was ro.
         Starting Flush Journal to Persistent Storage...
[  OK  ] Found device /dev/ttyPS0.
[  OK  ] Reached target Sound Card.
[  OK  ] Started Flush Journal to Persistent Storage.
         Starting Create Volatile Files and Directories...
[  OK  ] Started Create Volatile Files and Directories.
[  OK  ] Started LSB: Raise network interfaces..
[  OK  ] Created slice system-ifup.slice.
[  OK  ] Started ifup for sit0.
         Starting ifup for sit0...
[  OK  ] Started ifup for can0.
         Starting ifup for can0...
         Starting Network Time Synchronization...
         Starting Update UTMP about System Boot/Shutdown...
[  OK  ] Started Update UTMP about System Boot/Shutdown.
[  OK  ] Started Network Time Synchronization.
[  OK  ] Reached target System Time Synchronized.
[  OK  ] Reached target System Initialization.
[  OK  ] Reached target Timers.
[  OK  ] Listening on D-Bus System Message Bus Socket.
[  OK  ] Listening on OpenBSD Secure Shell server socket.
[  OK  ] Reached target Sockets.
[  OK  ] Reached target Basic System.
         Starting Login Service...
         Starting LSB: Load kernel modules needed to enable cpufreq scaling...
         Starting LSB: Platform initscript...
[  OK  ] Reached target Containers.
Running Platform Init
         Starting Initialize hardware monitoring sensors...
         Starting WPA supplicant...
         Starting Provide limited super user privileges to specific users...
         Starting Permit User Sessions...
         Starting LSB: Set the CPU Frequency Scaling governor to "ondemand"...
         Starting System Logging Service...
         Starting LSB: Xen daemons...
[  OK  ] Started Regular background program processing daemon.
         Starting Regular background program processing daemon...
         Starting Network Manager...
         Starting D-Bus System Message Bus...
[  OK  ] Started ifup for eth1.
         Starting ifup for eth1...
[  OK  ] Started LSB: Load kernel modules needed to enable cpufreq scaling.
[  OK  ] Started Provide limited super user privileges to specific users.
[  OK  ] Started Permit User Sessions.
[  OK  ] Started LSB: Set the CPU Frequency Scaling governor to "ondemand".
[  OK  ] Started LSB: Xen daemons.
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Started WPA supplicant.
[  OK  ] Started Initialize hardware monitoring sensors.
[  OK  ] Started System Logging Service.
         Starting Network Service...
         Starting LSB: Start/stop secondary xen domains...
         Starting LSB: set CPUFreq kernel parameters...
[  OK  ] Started Login Service.
[  OK  ] Started LSB: Start/stop secondary xen domains.
[  OK  ] Started LSB: set CPUFreq kernel parameters.
[  OK  ] Started Network Service.
         Starting Network Name Resolution...
[  OK  ] Started Network Name Resolution.
         Starting Authenticate and Authorize Users to Run Privileged Tasks...
[  OK  ] Started Authenticate and Authorize Users to Run Privileged Tasks.
[  OK  ] Started Network Manager.
[  OK  ] Reached target Network.
         Starting /etc/rc.local Compatibility...
         Starting Network Manager Wait Online...
[  OK  ] Stopped OpenBSD Secure Shell server.
[  OK  ] Started OpenBSD Secure Shell server.
         Starting OpenBSD Secure Shell server...
[  OK  ] Stopped LSB: start Samba SMB/CIFS daemon (smbd).
         Starting LSB: start Samba SMB/CIFS daemon (smbd)...
[  OK  ] Started LSB: Platform initscript.
[  OK  ] Closed OpenBSD Secure Shell server socket.
[  OK  ] Stopped OpenBSD Secure Shell server.
[  OK  ] Started OpenBSD Secure Shell server.
         Starting OpenBSD Secure Shell server...
[  OK  ] Started LSB: start Samba SMB/CIFS daemon (smbd).
[  OK  ] Started /etc/rc.local Compatibility.
[  OK  ] Started Getty on tty1.
         Starting Getty on tty1...
[  OK  ] Started Serial Getty on ttyPS0.
         Starting Serial Getty on ttyPS0...
[  OK  ] Reached target Login Prompts.

Ubuntu 15.04 linaro-developer ttyPS0

linaro-developer login: root (automatic login)

Last login: Fri Jan  8 23:28:18 UTC 2021 on ttyPS0
root@linaro-developer:~# ps aux
USER       PID %CPU %MEM    VSZ   RSS TTY      STAT START   TIME COMMAND
root         1  1.8  0.0   5084  3712 ?        Ss   05:44   0:02 /sbin/init earl
root         2  0.0  0.0      0     0 ?        S    05:44   0:00 [kthreadd]
root         3  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/0:0]
root         4  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/0:0H]
root         5  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/u8:0]
root         6  0.0  0.0      0     0 ?        I<   05:44   0:00 [mm_percpu_wq]
root         7  0.0  0.0      0     0 ?        S    05:44   0:00 [ksoftirqd/0]
root         8  0.0  0.0      0     0 ?        I    05:44   0:00 [rcu_sched]
root         9  0.0  0.0      0     0 ?        I    05:44   0:00 [rcu_bh]
root        10  0.0  0.0      0     0 ?        S    05:44   0:00 [migration/0]
root        11  0.0  0.0      0     0 ?        S    05:44   0:00 [cpuhp/0]
root        12  0.0  0.0      0     0 ?        S    05:44   0:00 [cpuhp/1]
root        13  0.0  0.0      0     0 ?        S    05:44   0:00 [migration/1]
root        14  0.0  0.0      0     0 ?        S    05:44   0:00 [ksoftirqd/1]
root        15  1.6  0.0      0     0 ?        I    05:44   0:02 [kworker/1:0]
root        16  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/1:0H]
root        17  0.0  0.0      0     0 ?        S    05:44   0:00 [cpuhp/2]
root        18  0.0  0.0      0     0 ?        S    05:44   0:00 [migration/2]
root        19  0.0  0.0      0     0 ?        S    05:44   0:00 [ksoftirqd/2]
root        20  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/2:0]
root        21  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/2:0H]
root        22  0.0  0.0      0     0 ?        S    05:44   0:00 [cpuhp/3]
root        23  0.0  0.0      0     0 ?        S    05:44   0:00 [migration/3]
root        24  0.0  0.0      0     0 ?        S    05:44   0:00 [ksoftirqd/3]
root        25  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/3:0]
root        26  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/3:0H]
root        27  0.0  0.0      0     0 ?        S    05:44   0:00 [kdevtmpfs]
root        28  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/u8:1]
root        32  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/u8:2]
root        37  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/2:1]
root        38  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/3:1]
root        56  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/0:1]
root        60  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/1:1]
root       433  0.0  0.0      0     0 ?        S    05:44   0:00 [oom_reaper]
root       434  0.0  0.0      0     0 ?        I<   05:44   0:00 [writeback]
root       436  0.0  0.0      0     0 ?        S    05:44   0:00 [kcompactd0]
root       437  0.0  0.0      0     0 ?        SN   05:44   0:00 [khugepaged]
root       438  0.0  0.0      0     0 ?        I<   05:44   0:00 [crypto]
root       440  0.0  0.0      0     0 ?        I<   05:44   0:00 [kblockd]
root       478  0.0  0.0      0     0 ?        I<   05:44   0:00 [edac-poller]
root       502  0.0  0.0      0     0 ?        I<   05:44   0:00 [cfg80211]
root       506  0.0  0.0      0     0 ?        I<   05:44   0:00 [watchdogd]
root       588  0.0  0.0      0     0 ?        I<   05:44   0:00 [rpciod]
root       589  0.0  0.0      0     0 ?        I<   05:44   0:00 [xprtiod]
root       603  0.0  0.0      0     0 ?        S    05:44   0:00 [kauditd]
root       609  0.0  0.0      0     0 ?        S    05:44   0:00 [kswapd0]
root       610  0.0  0.0      0     0 ?        S    05:44   0:00 [ecryptfs-kthre
root       611  0.0  0.0      0     0 ?        I<   05:44   0:00 [nfsiod]
root      1295  0.0  0.0      0     0 ?        S    05:44   0:00 [spi0]
root      1560  0.0  0.0      0     0 ?        S    05:44   0:00 [kpktgend_0]
root      1561  0.0  0.0      0     0 ?        S    05:44   0:00 [kpktgend_1]
root      1562  0.0  0.0      0     0 ?        S    05:44   0:00 [kpktgend_2]
root      1563  0.0  0.0      0     0 ?        S    05:44   0:00 [kpktgend_3]
root      1564  0.0  0.0      0     0 ?        I<   05:44   0:00 [ipv6_addrconf]
root      1568  0.0  0.0      0     0 ?        S<   05:44   0:00 [krfcommd]
root      1593  0.0  0.0      0     0 ?        S    05:44   0:00 [irq/44-fd4a000
root      1594  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/1:2]
root      1619  0.0  0.0      0     0 ?        S    05:44   0:00 [scsi_eh_0]
root      1621  0.0  0.0      0     0 ?        I<   05:44   0:00 [scsi_tmf_0]
root      1622  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/1:3]
root      1625  0.0  0.0      0     0 ?        S    05:44   0:00 [scsi_eh_1]
root      1626  0.0  0.0      0     0 ?        I<   05:44   0:00 [scsi_tmf_1]
root      1629  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/u8:3]
root      1647  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/u8:4]
root      1792  0.0  0.0      0     0 ?        S    05:44   0:00 [irq/38-mmc0]
root      1805  0.0  0.0      0     0 ?        S    05:44   0:00 [mmcqd/0]
root      1811  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/0:1H]
root      1813  0.0  0.0      0     0 ?        S    05:44   0:00 [jbd2/mmcblk0p2
root      1814  0.0  0.0      0     0 ?        I<   05:44   0:00 [ext4-rsv-conve
root      1840  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/3:2]
root      2133  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/0:2]
root      2250  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/2:2]
root      2252  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/3:3]
root      2255  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/3:1H]
root      2257  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/2:3]
root      2358  0.0  0.0      0     0 ?        I    05:44   0:00 [kworker/0:3]
root      3226  0.1  0.0  11388  2968 ?        Ss   05:44   0:00 /lib/systemd/sy
root      3227  0.1  0.0   9972  2220 ?        Ss   05:44   0:00 /lib/systemd/sy
systemd+  3381  0.0  0.0  11896  1572 ?        Ssl  05:44   0:00 /lib/systemd/sy
root      3428  0.0  0.0   3048  1860 ?        Ss   05:44   0:00 /lib/systemd/sy
root      3443  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/2:1H]
root      3463  0.0  0.0   5076  3084 ?        Ss   05:44   0:00 /sbin/wpa_suppl
syslog    3475  0.0  0.0  30888  2068 ?        Ssl  05:44   0:00 /usr/sbin/rsysl
root      3488  0.0  0.0   4460  1928 ?        Ss   05:44   0:00 /usr/sbin/cron 
root      3490  0.1  0.2  77496 10344 ?        Ssl  05:44   0:00 /usr/sbin/Netwo
message+  3503  0.1  0.0   4596  2460 ?        Ss   05:44   0:00 /usr/bin/dbus-d
root      3505  0.0  0.0      0     0 ?        I<   05:44   0:00 [kworker/1:1H]
systemd+  3526  0.0  0.0   3292  1872 ?        Ss   05:44   0:00 /lib/systemd/sy
root      3530  0.0  0.1  35816  5036 ?        Ssl  05:44   0:00 /usr/lib/policy
root      3558  0.0  0.0   6676  3740 ?        Ss   05:44   0:00 /usr/sbin/sshd 
root      3565  0.0  0.2  30036 11200 ?        Ss   05:44   0:00 /usr/sbin/smbd 
root      3567  0.0  0.1  30036  5008 ?        S    05:44   0:00 /usr/sbin/smbd 
root      3572  0.0  0.0   1968  1320 tty1     Ss+  05:44   0:00 /sbin/agetty --
root      3573  0.0  0.0   6212  2452 ttyPS0   Ss   05:44   0:00 /bin/login -f  
root      3589  0.0  0.0   4592  3184 ?        Ss   05:44   0:00 /lib/systemd/sy
root      3591  0.0  0.0   6420  1372 ?        S    05:44   0:00 (sd-pam)       
root      3593  0.0  0.0   4432  2392 ttyPS0   S    05:44   0:00 -bash
root      3638  0.0  0.0  19712  3824 ?        Ss   05:44   0:00 /usr/sbin/nmbd 
root      3649  0.1  0.1  10724  4312 ?        Ss   05:45   0:00 sshd: root@nott
root      3660  0.0  0.0   1808  1280 ?        Ss   05:45   0:00 /usr/lib/openss
root      3826  0.0  0.0   4224  1620 ttyPS0   R+   05:46   0:00 ps aux
root@linaro-developer:~# cd /home/analog/adrv9001_server/resources/Adi.Adrv9001. Server/
root@linaro-developer:/home/analog/adrv9001_server/resources/Adi.Adrv9001.Server## ls
Adrv9001Server_B0_39.0.7  Adrv9001Server_C0_39.0.7
root@linaro-developer:/home/analog/adrv9001_server/resources/Adi.Adrv9001.Server## ./Adrv9001Server_B0_39.0.7 
Segmentation fault
root@linaro-developer:/home/analog/adrv9001_server/resources/Adi.Adrv9001.Server## 

I would appreciate it if someone could help me.

 

Parents
  • Hi Mori,

    To the best of my knowledge the ZCU102 board is not fully supported yet, this platform should be supported soon though. The guide posted on EngineerZone Documents does mention that it has not been supported as of the Day 13 release, however we have not nailed down yet which release will support it.

    There is one issue with your setup however, you have the clock input on the far right of the board set to External, rather than Internal. Flip the switch on the far right of the board, between the SMA connector and the standoff, to the other end. This should allow the on board clock to be used by the ADRV9002. You can try making that edit and seeing if the device connects, do let us know if you're successful.

    One final thing to double check. You're trying to run the B0 server, make certain that it's the B0 silicon that you have. If it's C0 silicon then the B0 server will not work. If this is not an issue for your setup then it's likely the support isn't there yet for ZCU102.

    All the best,

    Oisín.

  • Hello,

    today I downloaded the tools and build the SDCARD.
    System is booting.

    But only the B0 server is listed.

    root@linaro-developer:/home/analog/adrv9001_server/resources/Adi.Adrv9001.Server#
    # ls
    Adrv9001Server_B0_37.0.0

    I used a virgin SDCard and a empty temp folder.

    It seems that mori has a newer version "Adrv9001Server_B0_39.0.7  Adrv9001Server_C0_39.07"

     Where can I get version 39 ?

    Best regard Stefan

Reply
  • Hello,

    today I downloaded the tools and build the SDCARD.
    System is booting.

    But only the B0 server is listed.

    root@linaro-developer:/home/analog/adrv9001_server/resources/Adi.Adrv9001.Server#
    # ls
    Adrv9001Server_B0_37.0.0

    I used a virgin SDCard and a empty temp folder.

    It seems that mori has a newer version "Adrv9001Server_B0_39.0.7  Adrv9001Server_C0_39.07"

     Where can I get version 39 ?

    Best regard Stefan

Children
  • Hello BPS,

    We have a guide for downloading and installing the SD card image on the EngineerZone forum. Navigate to the following link:

    https://ez.analog.com/wide-band-rf-transceivers/tes-gui-software-support-adrv9001-adrv9007/

    Then select the "Documents" tab in the blue ribbon at the top of the page:

    Select SD Card Image and select the guide you need.

    If you've followed this guide already and still it hasn't worked, then I suggest running it again. A few of our customers have noted a difficulty connecting to the server and getting a reliable download. Future revisions of Software will attempt to mitigate this, but following this guide should provide you with a stable SD card image.

    Do let me know how you get on with this!

    All the best,

    Oisín.

  • I followed the guid several times. But no success. 
    First of all. I can only find the Adrv9001Server_B0_37.0.0 server in:

    /home/analog/adrv9001_server/resources/Adi.Adrv9001.Server

    But I need the C0 version.

    The IP address 192.168.1.10 also not set.

    Have you any hint

  • I have the same issue. The RPC server seems to be erroring on the ZCU102:

    root@linaro-developer:/tmp# dmesg | grep -i adrv
    [ 139.517912] Adrv9001Server_[3716]: unhandled level 3 translation fault (11) at 0x00000023, esr 0x92000007, in Adrv9001Server_B0_39.0.7[8000+153000]
    [ 139.517930] CPU: 2 PID: 3716 Comm: Adrv9001Server_ Not tainted 4.14.0 #1

    -Travis

  • Hi BPS, Travis,

    There are a couple of reasons these issues could be occurring.

    1) During the SD card download you selected the "Legacy" option under Step 1. Doing so will download an SD card image that suits TES v.0.12.0 or older. Given the amount of changes between v0.12.0 and the current v0.14.0, the respective SD card images are completely incompatible.

    2) During the image formatting you selected the ZCU102 platform. This platform is not yet support, although that should change by the end of the month. Once the ZCU102 is support, try again. We should then be able to support C0 on that platform.

    Based on your descriptions of your issues it sounds like scenario 2 is what's what's happened? If you're both working on the newest version of SD card image this would explain your IP address issues. As of v0.14.0, we no longer assign a static IP address of 192.168.1.10. 

    DHCP is now enabled by default on the FPGA, which means that instead of using the static IP address 192.168.1.10, the FPGA now requests an IP address and a DHCP server (router) will give it an IP address. If there is no router i.e. when the FPGA is connected directly to your PC, it will fall back on the normal 192.168.1.10 address.

    Practically, this means you can connect as normal if you’re connected directly to the FPGA but if you connect your FPGA to a router, you must find the IP address and put that into TES.

    Let me know if this answers your questions.

    Best Regards,

    Oisín.