Post Go back to editing

GUI connection issue

I have trouble connecting to the board using the evaluation software (TES). Getting GUI pop-up error.

  • Hi again,

    This is a bit of a pernicious issue, it happens pretty rarely but the root cause is very hard to track down. I believe it's caused by some error being saved into a log file. Sadly the only solution I've found to be effective is to wipe TES and the SDK from the host machine (making sure to backup any files you wrote yourself or modified for your application) as well as deleting the .zip file downloaded from analog.com. Use the "Uninstall.exe" found in the TES folder to remove TES properly, before deleting the SDK. Download a new SDK and reinstall TES from scratch. This should give you a completely uncorrupted install.

    After that, before connecting TES to the ZC706, use PuTTY to confirm whether or not the Adi.Adrv9001.server folder is there. If it is, try to run the executable Adrv9001Server_B0_29.2.0 file. It may be called something else on your setup. With nothing connected, it should wait for something to try to connect to the server. At this point use TES to connect. If it isn't there, delete the /home/analog/adrv9001_server/resources folder, then try using TES to perform a "Force System Update" in the "File" dropdown menu in the top left corner. This should write a new folder with the server executable in it. Try to connect to TES normally first, then failing that try to connect by running the executable in PuTTY and then connecting through TES.

    Failing all of that, your best bet is a clean build of everything. New SDK, new TES and new SD card image. Before trying any of this be certain to have backed up any essential filesI do apologize that this debug guide is convoluted, long and not really certain of itself, however this particular issue is not always an easy one to fix. Sometimes just reinstalling TES will fix everything and there'll be no need for the long and difficult debug process. Other times you'll be deleting and reinstalling things for a long time and then it'll work with no explanation.

    The Documents Tab for this forum has a guide for reimaging the SD card, do give it a look also if you run into a lot of issues. Do also let me know if there's more questions I can answer.

    Best Regards,

    Oisín.

  • Hi Oisin,

    Please see the photo below, it's used the "for ADRV9001 TES software R0.1 2020.07" SD Card, from the purchase box.

    When run the "Adrv9001Server_B0_29.2.0" file, it's still not connect to the TES.

    If Used the Website download "adrv9001-tes-sdcard.zip" image,

    "Failed to start load kernel modules " Error message will still appear, try using TES to perform a "Force System Update", the folder and Adrv9001Server_B0_29.2.0 file finally appeared.

    But run the "Adrv9001Server_B0_29.2.0" file, show below

    I still can not connect to TES.

  • Hi Again,

    I've had a chat with the team for more solutions to this issue. The next things to check are the firewall and the server. Make certain there's nothing on your laptop / pc that's interfering with traffic over the ethernet port. If there is you'll need to find a way to disable it and allow ethernet traffic.

    Then to check the server, use PuTTY to perform the following commands:

    "ps -x | grep server" -> To locate the PID of the Server. It should also confirm if the server is running at all. If it is not running, try to start it again.

    "kill -9 <PID of server>" -> If the server is running, use this command to kill it and try running it again.

    Do let me know if any of this works.

    Best Regards,

    Oisín.

  • Hi Oisin,

    I think it may not be a problem with ethernet. When I used the ZC706 + AD9375 EVB, the TES connection is OK.

    Is there anything that needs to change or set when the ZC706 connect with ADRV9002? (example:  Vadj 1.8V?)

    Our ADRV9002 EVB red LED is Constantly On.....  UG-1828 says it auto adjust VAdj?

  • Hi Oisin,

    ADRV9002 EVB red LED is correct now, when the SW12 switch to close the number(1,2,3,4) position.

    But We still can not connect to TES....

  • Hi Oisin,

    Attached file is the putty LOG, please let me know if you have any idea, Thank you!!!

    =~=~=~=~=~=~=~=~=~=~=~= PuTTY log 2020.12.14 17:16:24 =~=~=~=~=~=~=~=~=~=~=~=
    �
    
    U-Boot 2018.01 (Aug 30 2018 - 18:22:43 +0530) Xilinx Zynq ZC706
    
    Model: Zynq ZC706 Development Board
    Board: Xilinx Zynq
    Silicon: v3.1
    I2C:   ready
    DRAM:  ECC disabled 1 GiB
    MMC:   sdhci@e0100000: 0 (SD)
    SF: Detected s25fl128s_64k with page size 512 Bytes, erase size 128 KiB, total 32 MiB
    In:    serial@e0001000
    Out:   serial@e0001000
    Err:   serial@e0001000
    Net:   ZYNQ GEM: e000b000, phyaddr 7, interface rgmii-id
    eth0: ethernet@e000b000
    Hit any key to stop autoboot:  3  2  1  0 
    Device: sdhci@e0100000
    Manufacturer ID: 2
    OEM: 544d
    Name: SA16G 
    Tran Speed: 50000000
    Rd Block Len: 512
    SD version 3.0
    High Capacity: Yes
    Capacity: 14.5 GiB
    Bus Width: 4-bit
    Erase Group Size: 512 Bytes
    reading uEnv.txt
    442 bytes read in 9 ms (47.9 KiB/s)
    Loaded environment from uEnv.txt
    Importing environment from SD ...
    Running uenvcmd ...
    Copying Linux from SD to RAM...
    reading uImage
    3929656 bytes read in 230 ms (16.3 MiB/s)
    reading devicetree.dtb
    19738 bytes read in 15 ms (1.3 MiB/s)
    ** Unable to read file uramdisk.image.gz **
    ## Booting kernel from Legacy Image at 03000000 ...
       Image Name:   Linux-4.14.0-xilinx-00107-g45f98
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    3929592 Bytes = 3.7 MiB
       Load Address: 00008000
       Entry Point:  00008000
       Verifying Checksum ... OK
    ## Flattened Device Tree blob at 02a00000
       Booting using the fdt blob at 0x2a00000
       Loading Kernel Image ... OK
       Loading Device Tree to 1fff8000, end 1ffffd19 ... OK
    
    Starting kernel ...
    
    Booting Linux on physical CPU 0x0
    Linux version 4.14.0-xilinx-00107-g45f9852-dirty (mchandra@gomati.spd.analog.com) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11-rc1)) #4 SMP PREEMPT Tue Oct 2 00:25:12 IST 2018
    CPU: ARMv7 Processor [413fc090] revision 0 (ARMv7), cr=18c5387d
    CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
    OF: fdt: Machine model: Zynq ZC706 Development Board
    Memory policy: Data cache writealloc
    cma: Reserved 16 MiB at 0x3f000000
    random: fast init done
    percpu: Embedded 16 pages/cpu @ef7c8000 s32844 r8192 d24500 u65536
    Built 1 zonelists, mobility grouping on.  Total pages: 260608
    Kernel command line: console=ttyPS0,115200 root=/dev/mmcblk0p2 rw earlyprintk rootfstype=ext4 rootwait uio_pdrv_genirq.of_id="generic-uio"
    PID hash table entries: 4096 (order: 2, 16384 bytes)
    Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    Memory: 1012860K/1048576K available (6144K kernel code, 237K rwdata, 1544K rodata, 1024K init, 152K bss, 19332K reserved, 16384K cma-reserved, 245760K highmem)
    Virtual kernel memory layout:
        vector  : 0xffff0000 - 0xffff1000   (   4 kB)
        fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
        vmalloc : 0xf0800000 - 0xff800000   ( 240 MB)
        lowmem  : 0xc0000000 - 0xf0000000   ( 768 MB)
        pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
        modules : 0xbf000000 - 0xbfe00000   (  14 MB)
          .text : 0xc0008000 - 0xc0700000   (7136 kB)
          .init : 0xc0900000 - 0xc0a00000   (1024 kB)
          .data : 0xc0a00000 - 0xc0a3b500   ( 238 kB)
           .bss : 0xc0a3b500 - 0xc0a6164c   ( 153 kB)
    Preemptible hierarchical RCU implementation.
    	RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=2.
    	Tasks RCU enabled.
    RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
    NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
    efuse mapped to f0800000
    slcr mapped to f0802000
    L2C: platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C: DT/platform modifies aux control register: 0x72360000 -> 0x72760000
    L2C-310 erratum 769419 enabled
    L2C-310 enabling early BRESP for Cortex-A9
    L2C-310 full line of zeros enabled for Cortex-A9
    L2C-310 ID prefetch enabled, offset 1 lines
    L2C-310 dynamic clock gating enabled, standby mode enabled
    L2C-310 cache controller enabled, 8 ways, 512 kB
    L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76760001
    zynq_clock_init: clkc starts at f0802100
    Zynq clock init
    sched_clock: 64 bits at 333MHz, resolution 3ns, wraps every 4398046511103ns
    clocksource: arm_global_timer: mask: 0xffffffffffffffff max_cycles: 0x4ce07af025, max_idle_ns: 440795209040 ns
    Switching to timer-based delay loop, resolution 3ns
    clocksource: ttc_clocksource: mask: 0xffff max_cycles: 0xffff, max_idle_ns: 537538477 ns
    timer #0 at f080a000, irq=17
    Console: colour dummy device 80x30
    Calibrating delay loop (skipped), value calculated using timer frequency.. 666.66 BogoMIPS (lpj=3333333)
    pid_max: default: 32768 minimum: 301
    Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    CPU: Testing write buffer coherency: ok
    CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    Setting up static identity map for 0x100000 - 0x100060
    Hierarchical SRCU implementation.
    smp: Bringing up secondary CPUs ...
    CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    smp: Brought up 1 node, 2 CPUs
    SMP: Total of 2 processors activated (1333.33 BogoMIPS).
    CPU: All CPU(s) started in SVC mode.
    devtmpfs: initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
    clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    futex hash table entries: 512 (order: 3, 32768 bytes)
    pinctrl core: initialized pinctrl subsystem
    NET: Registered protocol family 16
    DMA: preallocated 256 KiB pool for atomic coherent allocations
    cpuidle: using governor ladder
    hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
    hw-breakpoint: maximum watchpoint size is 4 bytes.
    zynq-ocm f800c000.ocmc: ZYNQ OCM pool: 256 KiB @ 0xf0880000
    zynq-pinctrl 700.pinctrl: zynq pinctrl initialized
    e0001000.serial: ttyPS0 at MMIO 0xe0001000 (irq = 26, base_baud = 3125000) is a xuartps
    console [ttyPS0] enabled
    vgaarb: loaded
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    media: Linux media interface: v0.10
    Linux video capture interface: v2.00
    pps_core: LinuxPPS API ver. 1 registered
    pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    PTP clock support registered
    FPGA manager framework
    fpga-region fpga-full: FPGA Region probed
    Advanced Linux Sound Architecture Driver Initialized.
    clocksource: Switched to clocksource arm_global_timer
    NET: Registered protocol family 2
    TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    TCP: Hash tables configured (established 8192 bind 8192)
    UDP hash table entries: 512 (order: 2, 16384 bytes)
    UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    NET: Registered protocol family 1
    RPC: Registered named UNIX socket transport module.
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    hw perfevents: no interrupt-affinity property for /pmu@f8891000, guessing.
    hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
    workingset: timestamp_bits=30 max_order=18 bucket_order=0
    jffs2: version 2.2. (NAND) (SUMMARY)  © 2001-2006 Red Hat, Inc.
    bounce: pool size: 64 pages
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    io scheduler mq-deadline registered
    io scheduler kyber registered
    dma-pl330 f8003000.dmac: Loaded driver for PL330 DMAC-241330
    dma-pl330 f8003000.dmac: 	DBUFF-128x8bytes Num_Chans-8 Num_Peri-4 Num_Events-16
    brd: module loaded
    loop: module loaded
    libphy: Fixed MDIO Bus: probed
    CAN device driver interface
    libphy: MACB_mii_bus: probed
    macb e000b000.ethernet eth0: Cadence GEM rev 0x00020118 at 0xe000b000 irq 28 (00:0a:35:00:01:22)
    Marvell 88E1116R e000b000.ethernet-ffffffff:07: attached PHY driver [Marvell 88E1116R] (mii_bus:phy_addr=e000b000.ethernet-ffffffff:07, irq=POLL)
    e1000e: Intel(R) PRO/1000 Network Driver - 3.2.6-k
    e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-pci: EHCI PCI platform driver
    usbcore: registered new interface driver usb-storage
    chipidea-usb2 e0002000.usb: e0002000.usb supply vbus not found, using dummy regulator
    ULPI transceiver vendor/product ID 0x0424/0x0007
    Found SMSC USB3320 ULPI transceiver.
    ULPI integrity check: passed.
    ci_hdrc ci_hdrc.0: EHCI Host Controller
    ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
    ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 1 port detected
    i2c /dev entries driver
    cdns-i2c e0004000.i2c: 400 kHz mmio e0004000 irq 23
    si570 1-005d: registered, current frequency 148500000 Hz
    i2c i2c-0: Added multiplexed i2c bus 1
    i2c i2c-0: Added multiplexed i2c bus 2
    at24 3-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write
    i2c i2c-0: Added multiplexed i2c bus 3
    i2c i2c-0: Added multiplexed i2c bus 4
    rtc-pcf8563 5-0051: low voltage detected, date/time is not reliable.
    rtc-pcf8563 5-0051: rtc core: registered rtc-pcf8563 as rtc0
    i2c i2c-0: Added multiplexed i2c bus 5
    i2c i2c-0: Added multiplexed i2c bus 6
    at24 7-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write
    i2c i2c-0: Added multiplexed i2c bus 7
    i2c i2c-0: Added multiplexed i2c bus 8
    pca954x 0-0074: registered 8 multiplexed busses for I2C switch pca9548
    IR NEC protocol handler initialized
    IR RC5(x/sz) protocol handler initialized
    IR RC6 protocol handler initialized
    IR JVC protocol handler initialized
    IR Sony protocol handler initialized
    IR SANYO protocol handler initialized
    IR Sharp protocol handler initialized
    IR MCE Keyboard/mouse protocol handler initialized
    IR XMP protocol handler initialized
    cdns-wdt f8005000.watchdog: Xilinx Watchdog Timer at f0992000 with timeout 10s
    Xilinx Zynq CpuIdle Driver started
    sdhci: Secure Digital Host Controller Interface driver
    sdhci: Copyright(c) Pierre Ossman
    sdhci-pltfm: SDHCI platform and OF driver helper
    mmc0: SDHCI controller on e0100000.sdhci [e0100000.sdhci] using ADMA
    ledtrig-cpu: registered to indicate activity on CPUs
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    fpga_manager fpga0: Xilinx Zynq FPGA Manager registered
    NET: Registered protocol family 10
    Segment Routing with IPv6
    sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
    NET: Registered protocol family 17
    can: controller area network core (rev 20170425 abi 9)
    NET: Registered protocol family 29
    can: raw protocol (rev 20170425)
    can: broadcast manager protocol (rev 20170425 t)
    can: netlink gateway (rev 20170425) max_hops=1
    Registering SWP/SWPB emulation handler
    input: gpio_keys as /devices/soc0/gpio_keys/input/input0
    rtc-pcf8563 5-0051: low voltage detected, date/time is not reliable.
    rtc-pcf8563 5-0051: hctosys: unable to read the hardware clock
    of_cfs_init
    of_cfs_init: OK
    mmc0: new high speed SDHC card at address 1234
    mmcblk0: mmc0:1234 SA16G 14.5 GiB 
    ALSA device list:
     mmcblk0: p1 p2 p3
      No soundcards found.
    �EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    VFS: Mounted root (ext4 filesystem) on device 179:2.
    devtmpfs: mounted
    Freeing unused kernel memory: 1024K
    systemd[1]: Failed to insert module 'autofs4'
    
    Welcome to Ubuntu 15.04!
    
    Cannot add dependency job for unit org.freedesktop.resolve1.busname, ignoring: Unit org.freedesktop.resolve1.busname failed to load: No such file or directory.
    Cannot add dependency job for unit cups.service, ignoring: Unit cups.service failed to load: No such file or directory.
    [  OK  ] Created slice Root Slice.
    [  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
    [  OK  ] Listening on Journal Socket (/dev/log).
    [  OK  ] Created slice System Slice.
    [  OK  ] Created slice User and Session Slice.
    [  OK  ] Reached target Slices.
    [  OK  ] Listening on udev Control Socket.
    [  OK  ] Listening on Delayed Shutdown Socket.
    [  OK  ] Listening on networkd rtnetlink socket.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [  OK  ] Listening on udev Kernel Socket.
    [  OK  ] Listening on Journal Socket.
             Starting Load Kernel Modules...
    [  OK  ] Started Boot Process Profiler.
             Starting Boot Process Profiler...
             Starting udev Coldplug all Devices...
             Mounting Temporary Directory...
    [  OK  ] Started Braille Device Support.
             Starting Braille Device Support...
    [  OK  ] Started Read required files in advance.
             Starting Read required files in advance...
             Starting Setup Virtual Console...
    [  OK  ] Reached target Encrypted Volumes.
    [  OK  ] Reached target Swap.
             Starting Increase datagram queue length...
    [  OK  ] Created slice system-getty.slice.
             Starting Nameserver information manager...
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Reached target Remote File Systems (Pre).
             Starting Create Static Device Nodes in /dev...
    [FAILED] Failed to start Load Kernel Modules.
    See "systemctl status systemd-modules-load.service" for details.
    systemd-modules-load.service failed.
    systemd-bootchart.service failed.
             Starting Apply Kernel Variables...
             Mounting Configuration File System...
    [  OK  ] Started Setup Virtual Console.
    [  OK  ] Mounted Configuration File System.
    [  OK  ] Mounted Temporary Directory.
    [  OK  ] Started Increase datagram queue length.
    ureadahead.service failed.
    [  OK  ] Started Remount Root and Kernel File Systems.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Started Nameserver information manager.
    [  OK  ] Started udev Coldplug all Devices.
             Starting udev Kernel Device Manager...
    [  OK  ] Reached target Local File Systems (Pre).
             Starting Load/Save Random Seed...
    [  OK  ] Listening on Syslog Socket.
             Starting Journal Service...
    [  OK  ] Reached target Local File Systems.
             Starting Wait for all "auto" /etc/n... up for network-online.target...
             Starting Tell Plymouth To Write Out Runtime Data...
             Starting Set console keymap...
    [  OK  ] Reached target Remote File Systems.
    [  OK  ] Started Load/Save Random Seed.
             Starting LSB: Raise network interfaces....
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Journal Service.
             Starting Flush Journal to Persistent Storage...
    [  OK  ] Started udev Kernel Device Manager.
    [  OK  ] Reached target Paths.
             Starting Copy rules generated while the root was ro...
    [  OK  ] Started Set console keymap.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started Copy rules generated while the root was ro.
    [  OK  ] Found device /dev/ttyPS0.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Create Volatile Files and Directories.
             Starting Update UTMP about System Boot/Shutdown...
             Starting Network Time Synchronization...
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Created slice system-ifup.slice.
    [  OK  ] Started ifup for eth0.
             Starting ifup for eth0...
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Started ifup for sit0.
             Starting ifup for sit0...
    [  OK  ] Started LSB: Raise network interfaces..
    [  OK  ] Started Wait for all "auto" /etc/ne...be up for network-online.target.
    [  OK  ] Reached target System Initialization.
    [  OK  ] Listening on OpenBSD Secure Shell server socket.
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
             Starting LSB: Speech Dispatcher...
             Starting Permit User Sessions...
    [  OK  ] Reached target Containers.
             Starting LSB: Platform initscript...
    [  OK  ] Started Run anacron jobs.
    Running Platform Init
             Starting Run anacron jobs...
             Starting Enable support for additional executable binary formats...
             Starting Accounts Service...
             Starting LSB: Set the CPU Frequency Scaling governor to "ondemand"...
             Starting LSB: Xen daemons...
             Starting Restore /etc/resolv.conf i...e the ppp link was shut down....
             Starting Initialize hardware monitoring sensors...
    [  OK  ] Started Regular background program processing daemon.
             Starting Regular background program processing daemon...
             Starting Network Manager...
             Starting Provide limited super user privileges to specific users...
             Starting LSB: Load kernel modules needed to enable cpufreq scaling...
             Starting LSB: automatic crash report generation...
             Starting WPA supplicant...
             Starting Avahi mDNS/DNS-SD Stack...
             Starting System Logging Service...
    [  OK  ] Started Cgroup management daemon.
             Starting Cgroup management daemon...
             Starting D-Bus System Message Bus...
             Starting Login Service...
    [  OK  ] Started LSB: Speech Dispatcher.
    [  OK  ] Started Permit User Sessions.
    [  OK  ] Started Enable support for additional executable binary formats.
    [  OK  ] Started LSB: Set the CPU Frequency Scaling governor to "ondemand".
    [  OK  ] Started LSB: Xen daemons.
    [  OK  ] Started Restore /etc/resolv.conf if...ore the ppp link was shut down..
    [  OK  ] Started Provide limited super user privileges to specific users.
    [  OK  ] Started LSB: Load kernel modules needed to enable cpufreq scaling.
    [  OK  ] Started LSB: automatic crash report generation.
    [  OK  ] Started D-Bus System Message Bus.
    Switching VADJ from 2.5V to 1.8V
    [  OK  ] Started WPA supplicant.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Started Initialize hardware monitoring sensors.
    [  OK  ] Started System Logging Service.
    fpga_manager fpga0: Error requesting firmware system_top.bit.bin
    failed to load fpga image
    OF: overlay: of_overlay_create: Pre-apply notifier failed (err=-22)
    create_overlay: Failed to create overlay (err=-22)
    [  OK  ] Started Login Service.
             Starting Authenticate and Authorize Users to Run Privileged Tasks...
    [  OK  ] Started Make remote CUPS printers available locally.
             Starting Make remote CUPS printers available locally...
             Starting Network Service...
             Starting LSB: set CPUFreq kernel parameters...
             Starting LSB: Start/stop secondary xen domains...
             Starting Light Display Manager...
    [  OK  ] Started LSB: set CPUFreq kernel parameters.
    [  OK  ] Started LSB: Start/stop secondary xen domains.
    [  OK  ] Started Network Service.
    Unhandled fault: imprecise external abort (0x406) at 0xb6cab000
    pgd = ee48c000
    [b6cab000] *pgd=3ed6b831
    Internal error: Oops - BUG: 406 [#1] PREEMPT SMP ARM
    Modules linked in:
    CPU: 1 PID: 1750 Comm: cat Not tainted 4.14.0-xilinx-00107-g45f9852-dirty #4
    Hardware name: Xilinx Zynq Platform
    task: ef172d80 task.stack: ee4b0000
    PC is at xspi_read32+0x8/0xc
    LR is at xilinx_spi_probe+0x2c8/0x538
    pc : [<c03ff5a0>]    lr : [<c03ffdbc>]    psr: 600c0013
    sp : ee4b1ce0  ip : 00000000  fp : 00000000
    r10: c08118fd  r9 : f0b63000  r8 : eebc4e00
    r7 : ee6fd800  r6 : eebc4e10  r5 : 00000000  r4 : ee6fdb38
    r3 : c03ff598  r2 : 00000000  r1 : 600c0013  r0 : 00000000
    Flags: nZCv  IRQs on  FIQs on  Mode SVC_32  ISA ARM  Segment none
    Control: 18c5387d  Table: 2e48c04a  DAC: 00000051
    Process cat (pid: 1750, stack limit = 0xee4b0210)
    Stack: (0xee4b1ce0 to 0xee4b2000)
    1ce0: 00000000 eeb1f580 eeb1fdc0 c081bd2a 00000003 00000008 00000000 00000100
    1d00: c03ffaf4 eebc4e10 c0a1c574 00000000 c0a1c574 00000000 00000003 c03abbc0
    1d20: eebc4e10 c0a55858 c0a5585c c03aa708 00000000 ee4b1d68 c03aa8ac eebc4e44
    1d40: c0a55834 00000000 00000000 c03a9000 ef076f6c ee8c1538 eebc4e10 c0a18e68
    1d60: 00000001 c03aa490 eebc4e10 00000001 00000031 eebc4e10 c0a18e68 eebc4e10
    1d80: ef17a810 c03a9ae0 eebc4e10 eebc4e18 00000000 c03a82fc eebc4e10 400c0013
    1da0: 00000000 ffffffff eebc4e00 ef7f6048 00000000 00000000 ef17a810 00000008
    1dc0: ee50d108 c04f0948 ee4b1e4c ef17a800 00000005 ee4b1e4c c0a1bfb0 c04f1018
    1de0: c0a32e18 00000005 ffffffff 00000000 00000005 c013425c 00000005 c0a32f44
    1e00: ee4b1e4c ffffffff ee50d100 c0134620 00000000 00000005 ee4b1e4c eeabdd80
    1e20: eeabdd80 ef158294 eead3800 c013464c 00000000 00000005 ee4b1e4c c04f2a90
    1e40: eeabdd80 c04f2ad4 00000005 ef7f5ff8 ee50d980 ef7f62ac eeabdd80 c04f2b64
    1e60: 800c0013 c022a5b0 00000000 ee50d998 00000001 c04f2ea0 eeabdd80 ef7f62ac
    1e80: eeabdd80 00000000 ef158294 c04f3214 eead3a84 eead3800 c082f4c3 eead3800
    1ea0: ee50d100 c04ee978 ef158280 00000000 00000001 c04f78ec 00000000 014000c0
    1ec0: 00000000 c080f812 eead3800 00000000 ef158284 ef158294 ef7f72bc 00000000
    1ee0: 00000014 eead38c8 dfffc57c 00000036 eeef1d70 ee5a7000 00000000 ee5a6000
    1f00: 00000000 eeef1d70 eeaa3210 eeef1d70 eead7f08 c04f2150 00000109 ee5a7000
    1f20: ee5a6000 c04f21dc ee6381c0 00000001 00000000 eead7f00 eeef1d70 c022ba18
    1f40: eead7f00 eeef1d70 00000000 00000008 eedef220 c01d2cac 00000000 00000000
    1f60: 00000000 00000000 ef1731f8 ef172d80 eead7f00 c0a3c4d0 ee4b0000 00000000
    1f80: 00020000 c0131e94 c01070a4 ffffe000 ee4b1fb0 00000006 c01070a4 c010a344
    1fa0: b6f4bd60 b6f85390 00000000 c0106f40 00000000 80100000 fbad2004 b6eae79d
    1fc0: b6f4bd60 b6f85390 00000000 00000006 b6f4c0b4 00000000 00000000 00020000
    1fe0: b6ea76a9 bef71b64 b6eaf4f5 b6eeb036 400c0030 00000001 00000000 00000000
    [<c03ff5a0>] (xspi_read32) from [<c03ffdbc>] (xilinx_spi_probe+0x2c8/0x538)
    [<c03ffdbc>] (xilinx_spi_probe) from [<c03abbc0>] (platform_drv_probe+0x50/0x9c)
    [<c03abbc0>] (platform_drv_probe) from [<c03aa708>] (driver_probe_device+0x1ec/0x2b0)
    [<c03aa708>] (driver_probe_device) from [<c03a9000>] (bus_for_each_drv+0x84/0x8c)
    [<c03a9000>] (bus_for_each_drv) from [<c03aa490>] (__device_attach+0x98/0x100)
    [<c03aa490>] (__device_attach) from [<c03a9ae0>] (bus_probe_device+0x28/0x80)
    [<c03a9ae0>] (bus_probe_device) from [<c03a82fc>] (device_add+0x400/0x500)
    [<c03a82fc>] (device_add) from [<c04f0948>] (of_platform_device_create_pdata+0x7c/0xa0)
    [<c04f0948>] (of_platform_device_create_pdata) from [<c04f1018>] (of_platform_notify+0x6c/0xe0)
    [<c04f1018>] (of_platform_notify) from [<c013425c>] (notifier_call_chain+0x40/0x64)
    [<c013425c>] (notifier_call_chain) from [<c0134620>] (__blocking_notifier_call_chain+0x40/0x58)
    [<c0134620>] (__blocking_notifier_call_chain) from [<c013464c>] (blocking_notifier_call_chain+0x14/0x1c)
    [<c013464c>] (blocking_notifier_call_chain) from [<c04f2a90>] (of_reconfig_notify+0x14/0x2c)
    [<c04f2a90>] (of_reconfig_notify) from [<c04f2ad4>] (of_property_notify+0x2c/0x34)
    [<c04f2ad4>] (of_property_notify) from [<c04f2b64>] (__of_changeset_entry_notify+0x88/0xa8)
    [<c04f2b64>] (__of_changeset_entry_notify) from [<c04f3214>] (__of_changeset_apply+0x9c/0xac)
    [<c04f3214>] (__of_changeset_apply) from [<c04f78ec>] (of_overlay_create+0x3e0/0x4dc)
    [<c04f78ec>] (of_overlay_create) from [<c04f2150>] (create_overlay+0x78/0xac)
    [<c04f2150>] (create_overlay) from [<c04f21dc>] (cfs_overlay_item_dtbo_write+0x58/0x88)
    [<c04f21dc>] (cfs_overlay_item_dtbo_write) from [<c022ba18>] (configfs_release_bin_file+0x50/0x84)
    [<c022ba18>] (configfs_release_bin_file) from [<c01d2cac>] (__fput+0xd8/0x1ac)
    [<c01d2cac>] (__fput) from [<c0131e94>] (task_work_run+0x9c/0xac)
    [<c0131e94>] (task_work_run) from [<c010a344>] (do_work_pending+0xa8/0xb0)
    [<c010a344>] (do_work_pending) from [<c0106f40>] (slow_work_pending+0xc/0x20)
    Code: e28cc004 eafffff1 e5900000 f57ff04f (e12fff1e) 
    ---[ end trace 51947515224cf2e7 ]---
    Unhandled fault: external abort on non-linefetch (0x018) at 0xb6f4f080
    pgd = ee48c000
    [b6f4f080] *pgd=3ece3831
    [  OK  ] Started Authenticate and Authorize Users to Run Privileged Tasks.
    [  OK  ] Started Accounts Service.
    [  OK  ] Started Network Manager.
    [  OK  ] Started Light Display Manager.
             Starting Network Manager Wait Online...
    [  OK  ] Reached target Network.
             Starting /etc/rc.local Compatibility...
             Starting Network Name Resolution...
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Started Network Manager Wait Online.
    [  OK  ] Started /etc/rc.local Compatibility.
             Starting Wait for Plymouth Boot Screen to Quit...
    [  OK  ] Reached target Network is Online.
             Starting LSB: start Samba NetBIOS nameserver (nmbd)...
             Starting LSB: start Samba daemons for the AD DC...
             Starting LSB: Tool to automatically...ubmit kernel crash signatures...
             Starting LSB: simple distributed compiler server...
    [  OK  ] Started Wait for Plymouth Boot Screen to Quit.
    [  OK  ] Started Getty on tty1.
             Starting Getty on tty1...
    [  OK  ] Started Serial Getty on ttyPS0.
             Starting Serial Getty on ttyPS0...
    [  OK  ] Reached target Login Prompts.
    [  OK  ] Started LSB: simple distributed compiler server.
    [  OK  ] Started LSB: Tool to automatically ... submit kernel crash signatures.
    
    
    Ubuntu 15.04 analog ttyPS0
    
    analog login: root (automatic login)
    
    
    Last login: Mon Dec 14 02:08:01 UTC 2020 on ttyPS0
    root@analog:~# 

    By the way, the ADP5056 normally have 1V0, 1V3 and 1V8 output? 

  • Hi Luke,

    Can you confirm for me that

    a) The FPGA is configured exactly as stated in the User Guide

    b) The Red LED remains off when the FPGA is fully configured (If it does not turn off then there's either an FPGA issue or a Linux kernel issue on the SD card)

    c) All Green LED's on the board light up. There's one close to the Red LED at the bottom of the board, a dim one in the middle of the board to indicate all power domains are okay, and 2 at the top of the board signifying that the VCTCXO is powered on and is selected using the adjacent switch.

    If we can confirm all of these and still the issue hasn't been fixed we'll know it's either a connection issue or a SW issue.

    Best Regards,

    Oisín.

  • Hi Oisin,

    The DS901 does not light, please see the video.

    Red
  • Hi Luke,

    That light is very dim, so do make certain it's definitely not turning on. If it's not turning on that means that the power domains for the ADRV9002 are not being set to the right level, which would explain your difficulties in connecting to it. We've experienced similar issues when setups were damaged by human error.

    The next thing we'll check is the inputs and outputs to the ADP5056 power supply chip. First check the three enable lines on R810, R807, R804 and then the power good output from the ADP5056 on R813. If the enable lines are all high and the output is low then there may be damage to this ADP5056 or to one of the surrounding components. These parts can be replaced if we confirm that there is indeed damage to them. One engineer noticed that a capacitor around the ADP5056 was causing a short to ground, go around the device and confirm that there's no damage to any component.

    If the 3 enable lines are not high that would indicate that power being delivered to the board, which would suggest an issue with the ZC706. That'd be surprising, but it could have happened.

    Let me know how this check goes.

    Best Regards,

    Oisín.

  • Hi Oisin,

    This is really disappointing!!!

    Three enable lines on R810, R807, R804 are all high(3.3V), and the Power good output on R813 is 4.8V.

    Channel3 (L803, D901) output voltage is 0.79V, Channel2 output voltage is 0.09V, Channel1 is 0V....

    And we could not found any capacitor short to ground that around the ADP5056.

    Are there any software control or feedback could cause this situation?