Hello,
I am using a custom board and need to set the RF Tx or Rx without entering the Radio Off state as it affects both the Tx and Rx.
I have read the details in UG-992 RF PLL FREQUENCY CHANGE PROCEDURE and it indicates that the radio must be in the "radio off" state.
I have read the section related to "Pin Mode" and it states that this mode allows independent control over the radio but nowhere does it explicitly indicate independent ability to change the frequency without entering Radio Off state.
Is there a way to change just the Tx, Rx or ORX frequency independently without having to enter "Radio Off"?
I am running an FDM system and need to change the Rx frequency without interrupting the Tx link.