Hello all,
I have AD9371 IC with Zynq ultrascale plus MPSoC on the custom board.
I want to enable TX LO Leakage external calibration through ORX2 ( ORX1 is not connected ).
Kindly tell me how can i do it.
Thanks
Mahima
Hello all,
I have AD9371 IC with Zynq ultrascale plus MPSoC on the custom board.
I want to enable TX LO Leakage external calibration through ORX2 ( ORX1 is not connected ).
Kindly tell me how can i do it.
Thanks
Mahima
I have updated the "Mykonos ARM Initialization Calibrations" section in ad9371.c file.
/*****************************************************/
/*** Mykonos ARM Initialization Calibrations ***/
/*****************************************************/
ret = ad9371_init_cal(phy, initCalMask);
dev_err(&phy->spi->dev, "initCalMask : (%x)", initCalMask);
if (ret != MYKONOS_ERR_OK) {
dev_err(&phy->spi->dev, "ad9371_init_cal error: %s (%d)",
getMykonosErrorMessage(ret), ret);
ret = -EFAULT;
goto out;
}
ret = ad9371_set_radio_state(phy, RADIO_ON);
if (ret) {
dev_err(&phy->spi->dev, "%s (%d)",
getMykonosErrorMessage(ret), ret);
//goto out_disable_obs_rx_clk;
}
ret = MYKONOS_setObsRxPathSource(mykDevice, OBS_RX2_TXLO);
dev_err(&phy->spi->dev, "MYKONOS_setObsRxPathSource setting to OBS_RX2_TXLO and function return value is : (%d)", ret);
if (ret) {
dev_err(&phy->spi->dev, "%s (%d)",
getMykonosErrorMessage(ret), ret);
ret = -EFAULT;
}
CMB_wait_ms(500);
//ad9371_init_cal(phy, TX_LO_LEAKAGE_EXTERNAL);
ret = ad9371_init_cal(phy, TX_LO_LEAKAGE_EXTERNAL);
if (ret != MYKONOS_ERR_OK) {
dev_err(&phy->spi->dev, "ad9371 TX_LO_LEAKAGE_EXTERNAL return value error: %s (%d)",
getMykonosErrorMessage(ret), ret);
ret = -EFAULT;
goto out;
}
ret = ad9371_set_radio_state(phy, RADIO_OFF);
if (ret) {
dev_err(&phy->spi->dev, "%s (%d)",
getMykonosErrorMessage(ret), ret);
//goto out_disable_obs_rx_clk;
}
ret = MYKONOS_getTxLolStatus(phy->mykDevice, TX1, &phy->txLolStatus[1]);
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus ret value : (%d)",ret);
if (ret) {
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus %s: %s (%d)", __func__,
getMykonosErrorMessage(ret), ret);
return ret;
}
if (&phy->txLolStatus[1].errorCode)
dev_err(&phy->spi->dev, "%s: error code (%d)\n", __func__, &phy->txLolStatus[1].errorCode);
if (&phy->txLolStatus[1].percentComplete)
dev_err(&phy->spi->dev, "%s: percentComplete (%d)\n", __func__, &phy->txLolStatus[1].percentComplete);
if (&phy->txLolStatus[1].performanceMetric)
dev_err(&phy->spi->dev, "%s: performanceMetric (%d)\n", __func__, &phy->txLolStatus[1].performanceMetric);
if (&phy->txLolStatus[1].iterCount)
dev_err(&phy->spi->dev, "%s: iterCount (%d)\n", __func__, &phy->txLolStatus[1].iterCount);
if (&phy->txLolStatus[1].updateCount)
dev_err(&phy->spi->dev, "%s: updateCount (%d)\n", __func__, &phy->txLolStatus[1].updateCount);
ret = MYKONOS_getTxLolStatus(phy->mykDevice, TX1, &phy->txLolStatus[2]);
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus ret value : (%d)",ret);
if (ret) {
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus %s: %s (%d)", __func__,
getMykonosErrorMessage(ret), ret);
return ret;
}
if (&phy->txLolStatus[2].errorCode)
dev_err(&phy->spi->dev, "%s: error code (%d)\n", __func__, &phy->txLolStatus[2].errorCode);
if (&phy->txLolStatus[2].percentComplete)
dev_err(&phy->spi->dev, "%s: percentComplete (%d)\n", __func__, &phy->txLolStatus[2].percentComplete);
if (&phy->txLolStatus[2].performanceMetric)
dev_err(&phy->spi->dev, "%s: performanceMetric (%d)\n", __func__, &phy->txLolStatus[2].performanceMetric);
if (&phy->txLolStatus[2].iterCount)
dev_err(&phy->spi->dev, "%s: iterCount (%d)\n", __func__, &phy->txLolStatus[2].iterCount);
if (&phy->txLolStatus[2].updateCount)
dev_err(&phy->spi->dev, "%s: updateCount (%d)\n", __func__, &phy->txLolStatus[2].updateCount);
Log details are:
[ 128.495192] ad9371 spi1.0: initCalMask : (7dff) [ 128.535615] ad9371 spi1.0: MYKONOS_setObsRxPathSource setting to OBS_RX2_TXLO and function return value is : (0) [ 129.063806] ERROR: 364: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode [ 129.073024] ERROR: 283: MYKONOS_waitInitCals() returned an ARM error [ 129.088077] ad9371 spi1.0: calsDoneLifetime 0x5DFF, calsDoneLastRun 0x5DFF, calsMinimum 0x4F, initErrCal 0x0, initErrCode 0x0 [ 129.131846] ad9371 spi1.0: initCalsCompleted 0x5DFF [ 129.136903] ad9371 spi1.0: errorWord 0x2, statusWord 0x0 [ 129.142248] ad9371 spi1.0: ArmCmdStatusByte 0x4 [ 129.156600] ad9371 spi1.0: TX_LO_LEAKAGE_EXTERNAL : (200) [ 129.184231] ad9371 spi1.0: Checking MYKONOS_getTxLolStatus ret value : (0) [ 129.191102] ad9371 spi1.0: ad9371_setup_cal_ms: error code (2063315820) [ 129.197720] ad9371 spi1.0: ad9371_setup_cal_ms: percentComplete (2063315824) [ 129.204761] ad9371 spi1.0: ad9371_setup_cal_ms: performanceMetric (2063315828) [ 129.211975] ad9371 spi1.0: ad9371_setup_cal_ms: iterCount (2063315832) [ 129.218494] ad9371 spi1.0: ad9371_setup_cal_ms: updateCount (2063315836) [ 129.236232] ad9371 spi1.0: Checking MYKONOS_getTxLolStatus ret value : (0) [ 129.243100] ad9371 spi1.0: ad9371_setup_cal_ms: error code (2063315840) [ 129.249714] ad9371 spi1.0: ad9371_setup_cal_ms: percentComplete (2063315844) [ 129.256759] ad9371 spi1.0: ad9371_setup_cal_ms: performanceMetric (2063315848) [ 129.263973] ad9371 spi1.0: ad9371_setup_cal_ms: iterCount (2063315852) [ 129.270492] ad9371 spi1.0: ad9371_setup_cal_ms: updateCount (2063315856) [ 129.286606] ad9371 spi1.0: deframerStatus (0x68) >From the above logs, initErrCal is coming as 0x0. This means " Tx baseband filter calibartion " error.initErrCode is coming as 0x0. This means " No error".
While running TX_LO_LEAKAGE_EXTERNAL calibration, I am getting above error. Please reply.
Hello, Thanks for the reply.
txObsSelect is already pulled to zero.
I am still not able to calibrate. Can you try on Eval board?
Hello,
I have tried on Eval board TRX 1 LOL External Calibration with ORX1.
It is working. But everytime whenever i am checking TX lol status, percentcomplete is showing 64 percent and iterCount is incrementing by 3.
Do i have to enable bist tone for callibration ?
Please suggest.
Hope you have connected the external path from TX1 to ORX1. What is the signal level and the LOl level that you are getting at the ORX output after running this cal?
Are you operating the chip in FDD mode?
Yes i have connected the external path from trx1 to orx1. Observation power is 12dbfs. Yes the chip is operating in FDD mode.
After running calibration . lo leakage is -85dbm at 1842.5MHz.
Please share with us the full log including iteration count , update count and percent complete. LOL update interval is 6sec, so please wait for some time before capturing the log.
Can you check the LOL levels before and after running the external LOL tracking cals. Then compare the levels between the two, to ensure if the tracking is running successfully.
Please check the below log:
ad9371_init_cal:574 initCalMask 200
[ 91.950033] ad9371_init_cal:578 Run mykError 0
[ 92.325376] ad9371_init_cal:583 Wait mykError 0
[ 92.341741] ad9371_init_cal:587 initCalStatus 200
[ 102.425863] ad9371 spi1.1: Checking MYKONOS_getTxLolStatus ret value : (0)
[ 102.432736] ad9371 spi1.1: ad9371_tx_lol_status: error code (0)
[ 102.438648] ad9371 spi1.1: ad9371_tx_lol_status: percentComplete (64)
[ 102.445079] ad9371 spi1.1: ad9371_tx_lol_status: performanceMetric (0)
[ 102.451601] ad9371 spi1.1: ad9371_tx_lol_status: iterCount (38)
[ 102.457518] ad9371 spi1.1: ad9371_tx_lol_status: updateCount (38)
[ 102.511627] ad9371 spi1.1: Checking Observation Power value : (2BF2)
"Can you check the LOL levels before and after running the external LOL tracking cals. "
- Earlier level was -82dBc and after calibration, level is around -85 and -86 dBc.
You can ignore percentage complete. That is status of current update and it varies as per what time we print the status. Iter count and update count are same means its working fine. LOL levels are as well good.
We don’t see an issue here.
Thanks
I have to test same calibration on our custom board with ORX2.
Is there any function to calculate ORX2 power level?
You can use the below API to measure the ORX dec power
|
You can use the below API to measure the ORX dec power
|
Thanks for the reply.
I have tried same configuration on our custom board. Hence TX1 LOL external calibration is working with ORX2.
But LOL is at -61dBc with respect to main frequency in bist mode. Is there any other ways to calibrate more?
When you are using the TX1 to ORX2 path for running the external LOL cals, are you seeing good LOL levels? When you are sending tone from FPGA ,are you seeing good LOL levels with TX1 to ORX2 external LOL calibration?
When you are sending the tone from internal TX NCO, what is the frequency of the tone?
Can you share a capture of the TX output when you are sending tone using TX NCO?
Sorry for the delayed response. I will share the snapshots.
The above figure shows bist tone after external LO calibration at TX1 through ORX2
The above figure shows bist tone before external LO calibration at TX1 through ORX2
You are seeing an improvement in LOL levels with External LOL tracking cal enabled. So, it confirms that the cal is running.
Can you share the status of the MYKONOS_getTxLolStatus when you are running TX1 to ORX2 external TXLOL cal? hope that the same loopback path is configured in GPIO settings as discussed before.
If you use TX1 to ORX1 path or TX2 to ORX2 path for running external TXLOL cal, how much LOL levels are you seeing?
Yes, improvement is there.
ad9371 spi1.1: Checking MYKONOS_getTxLolStatus ret value : (0)
ad9371 spi1.1: ad9371_tx_lol_status: error code (0)
ad9371 spi1.1: ad9371_tx_lol_status: percentComplete (64)
ad9371 spi1.1: ad9371_tx_lol_status: performanceMetric (0)
ad9371 spi1.1: ad9371_tx_lol_status: iterCount (38)
ad9371 spi1.1: ad9371_tx_lol_status: updateCount (38)
Yes, same loopback path is configured in GPIO settings.
We cannot run cal using ORX1 as on our custom board ORX1 is not connected.
From the LOL status, it can be confirmed that the external LOL tracking cal is running successfully.
As per datasheet, you should observe -81dBFs,or, -74dBm. You are observing an LOL of -70dBm, which looks good as per the output tone power level..
Can you increase the input power level and then check the LOL levels? It will give datasheet performance , Refer to the below conditions from datasheet and test:
3 dB RF and 3 dB digital attenuation, 40 kHz measurement BW