Hello all,
I have AD9371 IC with Zynq ultrascale plus MPSoC on the custom board.
I want to enable TX LO Leakage external calibration through ORX2 ( ORX1 is not connected ).
Kindly tell me how can i do it.
Thanks
Mahima
Hello all,
I have AD9371 IC with Zynq ultrascale plus MPSoC on the custom board.
I want to enable TX LO Leakage external calibration through ORX2 ( ORX1 is not connected ).
Kindly tell me how can i do it.
Thanks
Mahima
I have updated the "Mykonos ARM Initialization Calibrations" section in ad9371.c file.
/*****************************************************/
/*** Mykonos ARM Initialization Calibrations ***/
/*****************************************************/
ret = ad9371_init_cal(phy, initCalMask);
dev_err(&phy->spi->dev, "initCalMask : (%x)", initCalMask);
if (ret != MYKONOS_ERR_OK) {
dev_err(&phy->spi->dev, "ad9371_init_cal error: %s (%d)",
getMykonosErrorMessage(ret), ret);
ret = -EFAULT;
goto out;
}
ret = ad9371_set_radio_state(phy, RADIO_ON);
if (ret) {
dev_err(&phy->spi->dev, "%s (%d)",
getMykonosErrorMessage(ret), ret);
//goto out_disable_obs_rx_clk;
}
ret = MYKONOS_setObsRxPathSource(mykDevice, OBS_RX2_TXLO);
dev_err(&phy->spi->dev, "MYKONOS_setObsRxPathSource setting to OBS_RX2_TXLO and function return value is : (%d)", ret);
if (ret) {
dev_err(&phy->spi->dev, "%s (%d)",
getMykonosErrorMessage(ret), ret);
ret = -EFAULT;
}
CMB_wait_ms(500);
//ad9371_init_cal(phy, TX_LO_LEAKAGE_EXTERNAL);
ret = ad9371_init_cal(phy, TX_LO_LEAKAGE_EXTERNAL);
if (ret != MYKONOS_ERR_OK) {
dev_err(&phy->spi->dev, "ad9371 TX_LO_LEAKAGE_EXTERNAL return value error: %s (%d)",
getMykonosErrorMessage(ret), ret);
ret = -EFAULT;
goto out;
}
ret = ad9371_set_radio_state(phy, RADIO_OFF);
if (ret) {
dev_err(&phy->spi->dev, "%s (%d)",
getMykonosErrorMessage(ret), ret);
//goto out_disable_obs_rx_clk;
}
ret = MYKONOS_getTxLolStatus(phy->mykDevice, TX1, &phy->txLolStatus[1]);
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus ret value : (%d)",ret);
if (ret) {
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus %s: %s (%d)", __func__,
getMykonosErrorMessage(ret), ret);
return ret;
}
if (&phy->txLolStatus[1].errorCode)
dev_err(&phy->spi->dev, "%s: error code (%d)\n", __func__, &phy->txLolStatus[1].errorCode);
if (&phy->txLolStatus[1].percentComplete)
dev_err(&phy->spi->dev, "%s: percentComplete (%d)\n", __func__, &phy->txLolStatus[1].percentComplete);
if (&phy->txLolStatus[1].performanceMetric)
dev_err(&phy->spi->dev, "%s: performanceMetric (%d)\n", __func__, &phy->txLolStatus[1].performanceMetric);
if (&phy->txLolStatus[1].iterCount)
dev_err(&phy->spi->dev, "%s: iterCount (%d)\n", __func__, &phy->txLolStatus[1].iterCount);
if (&phy->txLolStatus[1].updateCount)
dev_err(&phy->spi->dev, "%s: updateCount (%d)\n", __func__, &phy->txLolStatus[1].updateCount);
ret = MYKONOS_getTxLolStatus(phy->mykDevice, TX1, &phy->txLolStatus[2]);
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus ret value : (%d)",ret);
if (ret) {
dev_err(&phy->spi->dev, "Checking MYKONOS_getTxLolStatus %s: %s (%d)", __func__,
getMykonosErrorMessage(ret), ret);
return ret;
}
if (&phy->txLolStatus[2].errorCode)
dev_err(&phy->spi->dev, "%s: error code (%d)\n", __func__, &phy->txLolStatus[2].errorCode);
if (&phy->txLolStatus[2].percentComplete)
dev_err(&phy->spi->dev, "%s: percentComplete (%d)\n", __func__, &phy->txLolStatus[2].percentComplete);
if (&phy->txLolStatus[2].performanceMetric)
dev_err(&phy->spi->dev, "%s: performanceMetric (%d)\n", __func__, &phy->txLolStatus[2].performanceMetric);
if (&phy->txLolStatus[2].iterCount)
dev_err(&phy->spi->dev, "%s: iterCount (%d)\n", __func__, &phy->txLolStatus[2].iterCount);
if (&phy->txLolStatus[2].updateCount)
dev_err(&phy->spi->dev, "%s: updateCount (%d)\n", __func__, &phy->txLolStatus[2].updateCount);
Log details are:
[ 128.495192] ad9371 spi1.0: initCalMask : (7dff) [ 128.535615] ad9371 spi1.0: MYKONOS_setObsRxPathSource setting to OBS_RX2_TXLO and function return value is : (0) [ 129.063806] ERROR: 364: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode [ 129.073024] ERROR: 283: MYKONOS_waitInitCals() returned an ARM error [ 129.088077] ad9371 spi1.0: calsDoneLifetime 0x5DFF, calsDoneLastRun 0x5DFF, calsMinimum 0x4F, initErrCal 0x0, initErrCode 0x0 [ 129.131846] ad9371 spi1.0: initCalsCompleted 0x5DFF [ 129.136903] ad9371 spi1.0: errorWord 0x2, statusWord 0x0 [ 129.142248] ad9371 spi1.0: ArmCmdStatusByte 0x4 [ 129.156600] ad9371 spi1.0: TX_LO_LEAKAGE_EXTERNAL : (200) [ 129.184231] ad9371 spi1.0: Checking MYKONOS_getTxLolStatus ret value : (0) [ 129.191102] ad9371 spi1.0: ad9371_setup_cal_ms: error code (2063315820) [ 129.197720] ad9371 spi1.0: ad9371_setup_cal_ms: percentComplete (2063315824) [ 129.204761] ad9371 spi1.0: ad9371_setup_cal_ms: performanceMetric (2063315828) [ 129.211975] ad9371 spi1.0: ad9371_setup_cal_ms: iterCount (2063315832) [ 129.218494] ad9371 spi1.0: ad9371_setup_cal_ms: updateCount (2063315836) [ 129.236232] ad9371 spi1.0: Checking MYKONOS_getTxLolStatus ret value : (0) [ 129.243100] ad9371 spi1.0: ad9371_setup_cal_ms: error code (2063315840) [ 129.249714] ad9371 spi1.0: ad9371_setup_cal_ms: percentComplete (2063315844) [ 129.256759] ad9371 spi1.0: ad9371_setup_cal_ms: performanceMetric (2063315848) [ 129.263973] ad9371 spi1.0: ad9371_setup_cal_ms: iterCount (2063315852) [ 129.270492] ad9371 spi1.0: ad9371_setup_cal_ms: updateCount (2063315856) [ 129.286606] ad9371 spi1.0: deframerStatus (0x68) >From the above logs, initErrCal is coming as 0x0. This means " Tx baseband filter calibartion " error.initErrCode is coming as 0x0. This means " No error".
While running TX_LO_LEAKAGE_EXTERNAL calibration, I am getting above error. Please reply.
Currently in the setup, TX1 data is coming at ORX2 input. No data is available at TX2.
txObsSelect is configured as zero.
Do i have to take care of anything else? Please suggest.
"You need to run external LOL init twice with switch position change for Tx1 and Tx2"
Is it still required when i am doing calibration for one path?
Thanks
Mahima
tx obs select output should be zero, for TX1 output feedback
Have you disabled the TX2 path during initialization using below API?
|
No, the external LOL cal should be run only once, if you need calibration for only one path
Thanks for the reply.
No i have not disabled TX2 path during initialization using this API init_txsettings.
Please tell where i can use this api and i did not find the same in ad9371.c file.
You need to edit the structure mykonosTxSettings_t to the required TX channel and then initialize the chip.
I have changed adi,tx-settings-tx-channels-enable from TX1_TX2 to TX1.
I am getting same error. Please check
[ 145.635551] ad9371_init_cal:583 initCalMask 200
[ 145.640187] ad9371_init_cal:587 Run mykError 0
[ 145.644689] ERROR: 364: MYKONOS_waitArmCmdStatus() exited due to ARM error for the desired ARM opcode
[ 145.653907] ERROR: 283: MYKONOS_waitInitCals() returned an ARM error
[ 145.660250] ad9371_init_cal:592 Wait mykError 11b
[ 145.675980] ad9371_init_cal:596 initCalStatus 5dff
[ 145.680763] ad9371_init_cal:599
[ 145.696031] ad9371 spi1.1: calsDoneLifetime 0x5DFF, calsDoneLastRun 0x5DFF, calsMinimum 0x4F, initErrCal 0x0, initErrCode 0x0
[ 145.739781] ad9371 spi1.1: initCalsCompleted 0x5DFF
[ 145.744835] ad9371 spi1.1: errorWord 0x2, statusWord 0x0
[ 145.750194] ad9371 spi1.1: ArmCmdStatusByte 0x4
As i do not have eval board, can you try on AD9371 eval board by modifying ad9371.c file?
Please check
Can you enable only ORX2 in the init config using the below API and initialize the chip and then check.,i.e, only TX1 and ORX2 should be enabled with a proper external feedback path between both of them.
mykonosObsRxSettings_t
If you disable the external TX LOL cal and then run the init, are you able to pass the initialization with TX1 and ORX2 enabled?
hi srimoyi,
AD9371_OF_PROP("adi,obs-settings-obs-rx-channels-enable", &phy->mykDevice->obsRx->obsRxChannelsEnable, MYK_ORX2);
AD9371_OF_PROP("adi,obs-settings-obs-rx-lo-source", &phy->mykDevice->obsRx->obsRxLoSource, 0);
AD9371_OF_PROP("adi,obs-settings-sniffer-pll-lo-frequency_hz", &phy->mykDevice->obsRx->snifferPllLoFrequency_Hz, 2600000000U);
AD9371_OF_PROP("adi,obs-settings-real-if-data", &phy->mykDevice->obsRx->realIfData, 0);
AD9371_OF_PROP("adi,obs-settings-default-obs-rx-channel", &phy->mykDevice->obsRx->defaultObsRxChannel, OBS_RX2_TXLO);
These are already set in ad9371.c file. Please tell if i have to set any other parameter.
"If you disable the external TX LOL cal and then run the init, are you able to pass the initialization with TX1 and ORX2 enabled? " - I will check
Can you check on Eval board TX LO External calibration with ORX2 ?
Thanks
Mahima
Just to confirm, in the tx obsselect, as you have given a zero input, have you pulled the gpio 0 pin to low which indicates to the ARM that the TX1 pin is routed.
Just to confirm, in the tx obsselect, as you have given a zero input, have you pulled the gpio 0 pin to low which indicates to the ARM that the TX1 pin is routed.
I did not understand your question completely.
Are you talking about useTx2EnablePin ?
No. GPIO 0 should be pulled to low so that the routing of the TX1 path for calibration is informed to the BBP.
Hello, Thanks for the reply.
txObsSelect is already pulled to zero.
I am still not able to calibrate. Can you try on Eval board?
Hello,
I have tried on Eval board TRX 1 LOL External Calibration with ORX1.
It is working. But everytime whenever i am checking TX lol status, percentcomplete is showing 64 percent and iterCount is incrementing by 3.
Do i have to enable bist tone for callibration ?
Please suggest.
Hope you have connected the external path from TX1 to ORX1. What is the signal level and the LOl level that you are getting at the ORX output after running this cal?
Are you operating the chip in FDD mode?
Yes i have connected the external path from trx1 to orx1. Observation power is 12dbfs. Yes the chip is operating in FDD mode.
After running calibration . lo leakage is -85dbm at 1842.5MHz.
Please share with us the full log including iteration count , update count and percent complete. LOL update interval is 6sec, so please wait for some time before capturing the log.
Can you check the LOL levels before and after running the external LOL tracking cals. Then compare the levels between the two, to ensure if the tracking is running successfully.
Please check the below log:
ad9371_init_cal:574 initCalMask 200
[ 91.950033] ad9371_init_cal:578 Run mykError 0
[ 92.325376] ad9371_init_cal:583 Wait mykError 0
[ 92.341741] ad9371_init_cal:587 initCalStatus 200
[ 102.425863] ad9371 spi1.1: Checking MYKONOS_getTxLolStatus ret value : (0)
[ 102.432736] ad9371 spi1.1: ad9371_tx_lol_status: error code (0)
[ 102.438648] ad9371 spi1.1: ad9371_tx_lol_status: percentComplete (64)
[ 102.445079] ad9371 spi1.1: ad9371_tx_lol_status: performanceMetric (0)
[ 102.451601] ad9371 spi1.1: ad9371_tx_lol_status: iterCount (38)
[ 102.457518] ad9371 spi1.1: ad9371_tx_lol_status: updateCount (38)
[ 102.511627] ad9371 spi1.1: Checking Observation Power value : (2BF2)
"Can you check the LOL levels before and after running the external LOL tracking cals. "
- Earlier level was -82dBc and after calibration, level is around -85 and -86 dBc.
You can ignore percentage complete. That is status of current update and it varies as per what time we print the status. Iter count and update count are same means its working fine. LOL levels are as well good.
We don’t see an issue here.