AD9371 PLL set up error

I am trying to set up the AD9371 on a custom board and am running into errors.  I used the Filter wizard v1.8 to create a custom profile and imported that into the TES software tool to export the c files for API set up.  When I run it goes error free until I get to the call to MYKONOS_setRfPllFrequency with TX_PLL as a parameter.  This function call returns the error MYKONOS_ERR_SETRFPLL_ARMERROR.  Stepping into the call it is the call to MYKONOS_waitArmCmdStatus that returns an error of MYKONOS_ERR_ARMCMDSTATUS_ARMERROR with a value for cmdStatusByte of 0x8.  A previous call to MYKONOS_setRfPllFrequency with RX_PLL as a parameter succeeds.

Parents Reply Children
  • I tried using a standard profile as well with the same results

    <profile AD9371 version=0 name=Rx 82, IQrate 100.000>
    <clocks>
    <deviceClock_kHz=100000>
    <clkPllVcoFreq_kHz=12000000>
    <clkPllVcoDiv=3>
    <clkPllHsDiv=4>
    </clocks>

    <rx>
    <adcDiv=1>
    <rxFirDecimation=2>
    <rxDec5Decimation=5>
    <enHighRejDec5=1>
    <rhb1Decimation=1>
    <iqRate_kHz=100000>
    <rfBandwidth_Hz=82000000>
    <rxBbf3dBCorner_kHz=82000>

    <filter FIR gain=-6 num=48>
    -7
    -30
    39
    55
    -77
    -122
    157
    218
    -275
    -374
    459
    600
    -725
    -932
    1114
    1421
    -1694
    -2174
    2655
    3470
    -4840
    -7545
    9702
    32260
    32260
    9702
    -7545
    -4840
    3470
    2655
    -2174
    -1694
    1421
    1114
    -932
    -725
    600
    459
    -374
    -275
    218
    157
    -122
    -77
    55
    39
    -30
    -7
    </filter>

    <adc-profile num=16>
    655
    475
    201
    98
    1280
    498
    1593
    284
    1061
    86
    643
    28
    48
    31
    18
    191
    </adc-profile>
    </rx>

    <obs>
    <adcDiv=1>
    <rxFirDecimation=2>
    <rxDec5Decimation=5>
    <enHighRejDec5=1>
    <rhb1Decimation=1>
    <iqRate_kHz=100000>
    <rfBandwidth_Hz=82000000>
    <rxBbf3dBCorner_kHz=41000>

    <filter FIR gain=0 num=48>
    -1
    -24
    22
    41
    -42
    -92
    92
    161
    -164
    -274
    280
    435
    -447
    -672
    695
    1019
    -1064
    -1556
    1676
    2523
    -2991
    -5635
    4397
    18298
    18298
    4397
    -5635
    -2991
    2523
    1676
    -1556
    -1064
    1019
    695
    -672
    -447
    435
    280
    -274
    -164
    161
    92
    -92
    -42
    41
    22
    -24
    -1
    </filter>

    <adc-profile num=16>
    655
    475
    201
    98
    1280
    498
    1593
    284
    1061
    86
    643
    28
    48
    31
    18
    191
    </adc-profile>

    <lpbk-adc-profile num=16>
    737
    439
    201
    98
    1280
    112
    1505
    53
    1081
    17
    667
    40
    48
    33
    19
    194
    </lpbk-adc-profile>
    </obs>

    <tx>
    <dacDiv=2.5>
    <txFirInterpolation=1>
    <thb1Interpolation=2>
    <thb2Interpolation=2>
    <txInputHbInterpolation=1>
    <iqRate_kHz=100000>
    <primarySigBandwidth_Hz=33000000>
    <rfBandwidth_Hz=82000000>
    <txDac3dBCorner_kHz=92000>
    <txBbf3dBCorner_kHz=41000>

    <filter FIR gain=6 num=16>
    36
    -248
    150
    -121
    -107
    892
    -2637
    20149
    -2637
    892
    -107
    -121
    150
    -248
    36
    0
    </filter>
    </tx>
    </profile>