I am trying to set up the AD9371 on a custom board and am running into errors. I used the Filter wizard v1.8 to create a custom profile and imported that into the TES software tool to export the c files for API set up. When I run it goes error free until I get to the call to MYKONOS_setRfPllFrequency with TX_PLL as a parameter. This function call returns the error MYKONOS_ERR_SETRFPLL_ARMERROR. Stepping into the call it is the call to MYKONOS_waitArmCmdStatus that returns an error of MYKONOS_ERR_ARMCMDSTATUS_ARMERROR with a value for cmdStatusByte of 0x8. A previous call to MYKONOS_setRfPllFrequency with RX_PLL as a parameter succeeds.
Please make sure that you follow the "RF PLL FREQUENCY CHANGE PROCEDURE" given in UG-992.
Are you using No-OS or Linux driver?
Can you please share the sequence you are following for RF PLL set?
I realized I wasn't using the latest version of the filter wizard so I downloaded v1.10 and had the same results
Make sure that you are using the latest version of the TES GUI from the below link:
https://www.analog.com/en/design-center/landing-pages/001/transceiver-evaluation-software.html
Are you able to program the chip successfully with the custom profile using TES GUI?
Are you able to initialize the device with any other standard profile?
Can you please share your custom profile?
I tried using a standard profile as well with the same results
<profile AD9371 version=0 name=Rx 82, IQrate 100.000> <clocks> <deviceClock_kHz=100000> <clkPllVcoFreq_kHz=12000000> <clkPllVcoDiv=3> <clkPllHsDiv=4> </clocks>
<rx> <adcDiv=1> <rxFirDecimation=2> <rxDec5Decimation=5> <enHighRejDec5=1> <rhb1Decimation=1> <iqRate_kHz=100000> <rfBandwidth_Hz=82000000> <rxBbf3dBCorner_kHz=82000>
<filter FIR gain=-6 num=48> -7 -30 39 55 -77 -122 157 218 -275 -374 459 600 -725 -932 1114 1421 -1694 -2174 2655 3470 -4840 -7545 9702 32260 32260 9702 -7545 -4840 3470 2655 -2174 -1694 1421 1114 -932 -725 600 459 -374 -275 218 157 -122 -77 55 39 -30 -7 </filter>
<adc-profile num=16> 655 475 201 98 1280 498 1593 284 1061 86 643 28 48 31 18 191 </adc-profile> </rx>
<obs> <adcDiv=1> <rxFirDecimation=2> <rxDec5Decimation=5> <enHighRejDec5=1> <rhb1Decimation=1> <iqRate_kHz=100000> <rfBandwidth_Hz=82000000> <rxBbf3dBCorner_kHz=41000>
<filter FIR gain=0 num=48> -1 -24 22 41 -42 -92 92 161 -164 -274 280 435 -447 -672 695 1019 -1064 -1556 1676 2523 -2991 -5635 4397 18298 18298 4397 -5635 -2991 2523 1676 -1556 -1064 1019 695 -672 -447 435 280 -274 -164 161 92 -92 -42 41 22 -24 -1 </filter>
<adc-profile num=16> 655 475 201 98 1280 498 1593 284 1061 86 643 28 48 31 18 191 </adc-profile>
<lpbk-adc-profile num=16> 737 439 201 98 1280 112 1505 53 1081 17 667 40 48 33 19 194 </lpbk-adc-profile> </obs>
<tx> <dacDiv=2.5> <txFirInterpolation=1> <thb1Interpolation=2> <thb2Interpolation=2> <txInputHbInterpolation=1> <iqRate_kHz=100000> <primarySigBandwidth_Hz=33000000> <rfBandwidth_Hz=82000000> <txDac3dBCorner_kHz=92000> <txBbf3dBCorner_kHz=41000>
<filter FIR gain=6 num=16> 36 -248 150 -121 -107 892 -2637 20149 -2637 892 -107 -121 150 -248 36 0 </filter> </tx></profile>
My profile doesn't use a clock that is compatible with the eval board so I can't load it using the TES GUI. I am using the latest
Can you please check whether the AD9528 device programmed properly and outputs the intended frequency at the reference clock input of AD9371?