AD9371 PLL set up error

I am trying to set up the AD9371 on a custom board and am running into errors.  I used the Filter wizard v1.8 to create a custom profile and imported that into the TES software tool to export the c files for API set up.  When I run it goes error free until I get to the call to MYKONOS_setRfPllFrequency with TX_PLL as a parameter.  This function call returns the error MYKONOS_ERR_SETRFPLL_ARMERROR.  Stepping into the call it is the call to MYKONOS_waitArmCmdStatus that returns an error of MYKONOS_ERR_ARMCMDSTATUS_ARMERROR with a value for cmdStatusByte of 0x8.  A previous call to MYKONOS_setRfPllFrequency with RX_PLL as a parameter succeeds.