I have a customer using the AD9371, No OS, on the ZC706 platform. He's looking for an example of a common.c file, is frustrated overall because there does not seem to be any example code available, no examples folder in the API .zip file.
This is direct from the customer;
Problem is that the No-OS API download does not contain an examples folder.
I understand that this and other files like common.c are to be customized for my custom target platform, but I am not there yet. I need to start with the a working platform which is the ZC706 ADVR9371reference platform. So if there was any code at all that works with the reference platform it would save a LOT of time and false starts trying to figure out how to get everything working from the ground up. That's one of the main purposes of a reference design, the other being for evaluation, which the TES application and IO Scope applications along with others provide nicely.
thanks...................Steve