Hi,
I have recently configured the boards: AD9082-FMCA-EBZ with ADS9 evaluation board using MatLab as provided by a user guide. I have two questions thou:
1) If i am configuring the boards using MatLab API, why do i need to upload the FPGA image? What is its role?
2) I am creating a 10 kHz single tone in MatLab. I then used the DAC to loop this signal to ADC and sample it and make sure i acquire the signal in MatLab again. I did acquire the signal successfully. But the frequency of the signal that was displayed in ACE software was 50 MHz which is different than the frequency i transmitted. The Fs used was 250 MHz. N.B. the signal i got in MatLab was 10 kHz.
Regards,