Post Go back to editing

AD9081 Configuration JRX link issue

Category: Choose a category

In the below configuration, when I try to test in ADS9+AD9081 The AD9081 JRX Link 0 status is off. Can anyone help me which part I am missing ?

RX =>

Mode 6, L=2,M=2,N=16,F=2,K=32

Rx Data Rate = 500Msps, Rx Clock Rate = 4 GHz, Rx Ref Clock = 500 MHz

Coarse = 4, Fine =2

TX =>

Mode 7, L=2,M=2,N=16,F=2,K=32

Rx Data Rate = 500Msps, Rx Clock Rate = 4 GHz, Rx Ref Clock = 500 MHz

Coarse = 4, Fine =2

Any help would be aprreciated. 

thanks

  • Hi,

    There appears to be a bug in the API for JRx mode 6 that prints that the link is down when it is not. Have you tried using DPG to check the link status and send a tone? When I ran the app with your parameters I saw the same link failure output statement, but in DPG the link is up and the tone sends normally. Let me know what you see.

    Best wishes