Hallo,
I wonder if the CDDC and FDDC of AD9988 should be set the same to CDUC and FDUC?
First, I set CDDC and FDDC = 2x3,CDUC and FDUC = 2x3,JTX and JRX link can both be established.
Second, CDDC and FDDC = 3x2,CDUC and FDUC = 2x3,JRX link can be established, JTX can't.
Third, CDDC and FDDC = 6x1,CDUC and FDUC = 6x1,JTX and JRX link can both be established.
My configuration parameters are as follows:
ADC clk= DAC clk =3686.4MHz,ADC JESD204C:L=8, M=8, F=2, S=1, K=128, E=1, N=16, NP=16
Is there any limit that CDDC and FDDC of AD9988 should be set the same to CDUC and FDUC?