Post Go back to editing

AD9082-FMCA-EBZ maximum FMC data rate

Category: Datasheet/Specs
Product Number: AD9082-FMCA-EBZ

Hi,

I'd like to use the AD9082-FMCA-EBZ with a custom FPGA board with FMC+ connector. UG-1829  (Evaluating the AD9081...) makes many references to using the AD9082-FMCA-EBZ with 24.75 Gb/s/lane link line rate. Am I right in thinking that the AD9082-FMCA-EBZ uses an FMC(not +) and is therefore only rated to 10Gb/s/lane?

In this case, should I anticipate there will be a certain amount of luck in using this board above this rate with any platform other than the supported ADS9-V2EBZ, or should I expect successful operation using the configurations in UG-1829 on arbitrary FMC+ platforms?

Thanks!

Jack