Post Go back to editing

EVAL-AD9082-FCMA vs -FCMB

Hello 

UG1578 of EVAL-AD9082 mentions FCMA and few times FCMB. 

Like Fig 36 pg. 38.

What is the difference(s) of FCMB to FCMA?

Parents
  • The FMCB board uses lower cost input baluns (i.e. Mini-Circuits TCM1-83x or LTCC balun option) as well as a different power supply distribution circuit based on the ADP5056 and LDO's.   Note that FMCB board either comes with AD9986 or AD9988 installed while FMCA board either comes with the AD9081 or AD9082 installed.

Reply
  • The FMCB board uses lower cost input baluns (i.e. Mini-Circuits TCM1-83x or LTCC balun option) as well as a different power supply distribution circuit based on the ADP5056 and LDO's.   Note that FMCB board either comes with AD9986 or AD9988 installed while FMCA board either comes with the AD9081 or AD9082 installed.

Children
No Data