Hi,
We have AD9082 with ADS9-V2EBZ and planning to add some modules in the system. But could not find any program button in ACE software.
Can you please help us in this?
Thanks and Regards
Pratibha
Hi,
We have AD9082 with ADS9-V2EBZ and planning to add some modules in the system. But could not find any program button in ACE software.
Can you please help us in this?
Thanks and Regards
Pratibha
please use these references to evaluate the AD9082 with ADS9-v2
AD9081-FMCA-EBZ/AD9082-FMCA-EBZ User Guide (Rev. PrA) (analog.com)
EVALUATING THE AD9082 / AD9081 / AD9986 / AD9988 Mixed-Signal Front-End…
I set up the system again today to send you the issue. however, i was able to configure the system successfully.
Thanks.
please use these references to evaluate the AD9082 with ADS9-v2
AD9081-FMCA-EBZ/AD9082-FMCA-EBZ User Guide (Rev. PrA) (analog.com)
Hi UmeshJ
Thanks for the references. However, i followed the same steps as the ones provided in the second link to configure AD9082 with ADS9-V2EBZ and i am getting
" Transaction Errors:
Error applying values: Can't stop eRPC server.
Error: Connection failed to establish within 5000 milliseconds. "
What can be the issue/s?
And one more point, from The 8 aligned lights on the AD9082, the first 5 are green, the 6th one is red and the other 2 are off. Why is that and maybe the former issue is due to this?
Hi, are you able to ping the erpc server?
I pinged the MicroZed and it did work.
I pinged the MicroZed and it did work.
can you please let me know where you are seeing this error? is this in the SSH terminal? is this in ACE? can you provide screenshots?
I set up the system again today to send you the issue. however, i was able to configure the system successfully.
Thanks.