AD9082 NCO sync

Hello,

I am trying to sync the NCO of CDDC0 and CDDC1 of AD9082.

From what i can tell, only the SYSREF sync option can do that, as the asynchronous reset via spi register is able to reset only one CDDC at the same time. 

I am using subclass 0 for JESD so i need SYSREF only to sync the NCO. 

I use a 1 MHz sysref signal output by the HMC7044 chip on the AD9082 FMC card

I tried to enable sysref logic with adi_ad9082_jesd_sysref_enable_set and  adi_ad9082_jesd_sysref_spi_enable_set.

I enable the sysref reset with sysref reset with adi_ad9082_adc_ddc_coarse_sync_enable_set and  adi_ad9082_adc_ddc_coarse_sync_next_set but it doesn't seem to be enough to sync the NCO.

I am checking COARSE_DDC_SYNC_EN_CLEAR flag, but i am not sure what it means. It is always 1 after i enable next sync with adi_ad9082_adc_ddc_coarse_sync_next_set.

I set the FDDC to ZIF to disable the channelizers NCO.

Thanks for helping me.

AD9082 is r2, i am using the bare metal no-OS driver