ZC706 or EVAL-TPG-ZYNQ3 initial set-up query

Hi,

A customer is trying to use the AD9081 on EVAL-TPG-ZYNQ3/ZC706  and posted... and connect it to a Linux PC, but I have some problems during the setup.

My target is to use the AD9081 card to receive 2 RF channels and stream them via PCIe (or ethernet) to my Linux PC in order to record the signals.

Furthermore, I would also like to transmit 2 RF channels from my Linux PC via PCIe (or ethernet).

Now my questions:

1: I don't know the correct setup of the 5 switches located on the board EVAL-TPG-ZYNQ3.

2: I have 2 different SD cards jointly provided with the boards: one SD card labeled AD-FMC-SDCARD, and the other labeled MxFE: Which one is the right one for my purpose? Or do I have to compile something else from your github repository?

3: I didn't find the drivers to comunicate with the board under Linux. Are they available? Is it easier if we use ACE software under Windows?

4: Do I have to use the USB port to setup the board at the switch-on or can I use the PCIe port?