Clock limitations on AD9528 not clear

In this document: https://ez.analog.com/docs/DOC-16454

It is listed with the following requirements:

• The PLL2 VCO frequency operates in range from 3450MHz to 4025MHz.

 

• Maximum frequency after the RF VCO divider (M1) is limited to 1000MHz.

However in the examples given, such as example 1, VCO is set to 3686.4 and M1 is set to 3. This would make the frequency after the RF VCO divider 1228.8, which should be violating that second rule. However, it is stated that that combination is acceptable, indicating that it is fine to exceed 1000 MHz.

Further, the RF VCO divider has listed values of /2, /3, and /4, however the datasheet lists the available divisions as /3,  /4, and /5. In general, if a /3 divider is used on a VCO operating in the range of 3450 to 4025 MHz, the resultant frequency should ALWAYS exceed 1000 MHz, making the /3 divider useless if that constraint exists.

Can you clarify what the limitations for this chip's settings are?

  • 0
    •  Analog Employees 
    on Jan 10, 2017 4:38 PM

    It is a mistake the point where the limitation is shown, it should be after channel divider and it is corrected now.

    As from datasheet OUT1 and OUT2 can be used till 1.25 GHz and all other OUT can you used till 1 GHz only.

    Yes the RF VCO divider values of /3, /4, and /5, same is corrected.

    Thanks for correcting.

  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:41 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin