Post Go back to editing

AD9364 TX/RX path latency

We have an application that is very sensitive to latency in both the TX and RX paths.

The AD9364 Reference Manual explains the latency due to the digital filters, but in addition to this latency, we are measuring an additional latency that is not explained in the data sheet or reference manual.

Our clock setup using the no-os drivers is as follows:
ad9361_set_trx_clock_chain: 960000000 480000000 240000000 120000000 60000000 60000000
ad9361_set_trx_clock_chain: 960000000 240000000 120000000 60000000 60000000 60000000

Looking at the AD9364 users guide "DIGITAL Rx BLOCK DELAY" it looks like I should be seeing a delay contribution from the digital filters of approx:
                  HB3           HB2           HB1   
RX path (2/240M) + (2/120M) + (7/60M) = 8.3ns + 16.6ns + 116ns = 140ns
TX path (2/120M) + (2/60M)  + 0             = 16.6ns + 33.8ns             =  50.4ns
 
= 190.4ns total delay for digital filters

I am using an ILA (logic analyzer) in our FPGA to capture the TX and RX data just before clocking in/out to the AD9364.  I am seeing a delay of approx. 800ns.

 

I know that the 190ns is only the digital filter delay.  Is there a description somewhere of what the source might be for the additional ~600ns delay I am measuring?

Most importantly for our application, is there anything that can be done to reduce the latency below the 800ns we are currently seeing?

 

Thank you for any assistance.

Parents
  • As an experiment, I also tried leaving the ADC / DAC data rates as is (480MS/s, 240MS/s respectively), but additionally bypassing RX-HB1 and TX-HB2 with a DATA_CLK now running at 240MHz vs 120MHz.

    After this change, the latency was cut in half, so it looks like whatever is introducing the additional latency is related to DATA_CLK and not the ADC/DAC clocks.

    The problem is, this would also seem to violate the maximum baseband rate of 61.44MHz even though UG-673 says DATA_CLK can go to 245.76MHz.

Reply
  • As an experiment, I also tried leaving the ADC / DAC data rates as is (480MS/s, 240MS/s respectively), but additionally bypassing RX-HB1 and TX-HB2 with a DATA_CLK now running at 240MHz vs 120MHz.

    After this change, the latency was cut in half, so it looks like whatever is introducing the additional latency is related to DATA_CLK and not the ADC/DAC clocks.

    The problem is, this would also seem to violate the maximum baseband rate of 61.44MHz even though UG-673 says DATA_CLK can go to 245.76MHz.

Children
No Data