Post Go back to editing

AD9364 TX/RX path latency

We have an application that is very sensitive to latency in both the TX and RX paths.

The AD9364 Reference Manual explains the latency due to the digital filters, but in addition to this latency, we are measuring an additional latency that is not explained in the data sheet or reference manual.

Our clock setup using the no-os drivers is as follows:
ad9361_set_trx_clock_chain: 960000000 480000000 240000000 120000000 60000000 60000000
ad9361_set_trx_clock_chain: 960000000 240000000 120000000 60000000 60000000 60000000

Looking at the AD9364 users guide "DIGITAL Rx BLOCK DELAY" it looks like I should be seeing a delay contribution from the digital filters of approx:
                  HB3           HB2           HB1   
RX path (2/240M) + (2/120M) + (7/60M) = 8.3ns + 16.6ns + 116ns = 140ns
TX path (2/120M) + (2/60M)  + 0             = 16.6ns + 33.8ns             =  50.4ns
 
= 190.4ns total delay for digital filters

I am using an ILA (logic analyzer) in our FPGA to capture the TX and RX data just before clocking in/out to the AD9364.  I am seeing a delay of approx. 800ns.

 

I know that the 190ns is only the digital filter delay.  Is there a description somewhere of what the source might be for the additional ~600ns delay I am measuring?

Most importantly for our application, is there anything that can be done to reduce the latency below the 800ns we are currently seeing?

 

Thank you for any assistance.

Parents
  • Here is the ILA capture using a simple impulse on TX and capturing RX.

    • DAC_I and DAC_Q are 12 bit slices of the axi_ad9361_lvds_if.v dac_data[47:0] nets
    • ADC_I and ADC_Q are 12 bit slices of the axi_ad9361_lvds_if.v adc_data[47:0] nets
    • tx_p_data_p is the 6 bit muxed tx data just as it is clocked into the ODDR/OBUFDS
    • rx_data_p is the 6 bit muxed rx data just as it is registered from the IDDR

    TX Impulse to RX using external RF loopback

    All signals are captured in the clock domain derived from the AD9364 DATA_CLK running at 120MHz.  We are using LVDS interface with DDR.

    The txp_data_p and rx_data_p are multiplexed between MSW/LSW I/Q.  The blue marker is placed at the start of the tx impulse as it is clocked into the ODDR.  The yellow marker is placed at the point where the data is clocked in from the IDDR.

    There is a delay of 72 clock pulses between them that corresponds to a latency of 600ns.

    For reference, below is a similar capture with the BIST data loopback enabled

    TX Impulse to RX using BIST data loopback

    Even the BIST data loopback has a latency of 17 clock cycles (142ns).  This is what leads me to believe there are significant sources of latency in addition to what we are calculating for just the digital filters.

    We just need to know what these additional sources of latency are, and if there is anything we can do about them.

Reply
  • Here is the ILA capture using a simple impulse on TX and capturing RX.

    • DAC_I and DAC_Q are 12 bit slices of the axi_ad9361_lvds_if.v dac_data[47:0] nets
    • ADC_I and ADC_Q are 12 bit slices of the axi_ad9361_lvds_if.v adc_data[47:0] nets
    • tx_p_data_p is the 6 bit muxed tx data just as it is clocked into the ODDR/OBUFDS
    • rx_data_p is the 6 bit muxed rx data just as it is registered from the IDDR

    TX Impulse to RX using external RF loopback

    All signals are captured in the clock domain derived from the AD9364 DATA_CLK running at 120MHz.  We are using LVDS interface with DDR.

    The txp_data_p and rx_data_p are multiplexed between MSW/LSW I/Q.  The blue marker is placed at the start of the tx impulse as it is clocked into the ODDR.  The yellow marker is placed at the point where the data is clocked in from the IDDR.

    There is a delay of 72 clock pulses between them that corresponds to a latency of 600ns.

    For reference, below is a similar capture with the BIST data loopback enabled

    TX Impulse to RX using BIST data loopback

    Even the BIST data loopback has a latency of 17 clock cycles (142ns).  This is what leads me to believe there are significant sources of latency in addition to what we are calculating for just the digital filters.

    We just need to know what these additional sources of latency are, and if there is anything we can do about them.

Children
No Data