AD9364 TX/RX path latency

We have an application that is very sensitive to latency in both the TX and RX paths.

The AD9364 Reference Manual explains the latency due to the digital filters, but in addition to this latency, we are measuring an additional latency that is not explained in the data sheet or reference manual.

Our clock setup using the no-os drivers is as follows:
ad9361_set_trx_clock_chain: 960000000 480000000 240000000 120000000 60000000 60000000
ad9361_set_trx_clock_chain: 960000000 240000000 120000000 60000000 60000000 60000000

Looking at the AD9364 users guide "DIGITAL Rx BLOCK DELAY" it looks like I should be seeing a delay contribution from the digital filters of approx:
                  HB3           HB2           HB1   
RX path (2/240M) + (2/120M) + (7/60M) = 8.3ns + 16.6ns + 116ns = 140ns
TX path (2/120M) + (2/60M)  + 0             = 16.6ns + 33.8ns             =  50.4ns
 
= 190.4ns total delay for digital filters

I am using an ILA (logic analyzer) in our FPGA to capture the TX and RX data just before clocking in/out to the AD9364.  I am seeing a delay of approx. 800ns.

 

I know that the 190ns is only the digital filter delay.  Is there a description somewhere of what the source might be for the additional ~600ns delay I am measuring?

Most importantly for our application, is there anything that can be done to reduce the latency below the 800ns we are currently seeing?

 

Thank you for any assistance.

Parents
  • Only the FIR can add more delay as it runs at lower rate and no of taps.

    if decimation is 1 but not bypassed which is possible then still it goes through FIR and you may be seeing this extra delay

    calculated for you configuration 

      TX Interpolation Filter order Delay RX Decimation Filter order Delay
    Data rate 6.00E+07       6.00E+07      
    FIR 6.00E+07 1 37 3.08E-07 6.00E+07 1 37 3.08E-07
    HB1 6.00E+07 1 0 0.00E+00 1.20E+08 2 14 5.83E-08
    HB2 1.20E+08 2 6 2.50E-08 2.40E+08 2 6 1.25E-08
    HB3 2.40E+08 2 4 8.33E-09 4.80E+08 2 4 4.17E-09
          TX Delay 3.4167E-07     RX delay 3.83E-07

    You can see total delay comes around 725 ns almost near to your measured value

    So please read 0x02 and 0x03 registers just to make sure FIR is bypassed?

Reply
  • Only the FIR can add more delay as it runs at lower rate and no of taps.

    if decimation is 1 but not bypassed which is possible then still it goes through FIR and you may be seeing this extra delay

    calculated for you configuration 

      TX Interpolation Filter order Delay RX Decimation Filter order Delay
    Data rate 6.00E+07       6.00E+07      
    FIR 6.00E+07 1 37 3.08E-07 6.00E+07 1 37 3.08E-07
    HB1 6.00E+07 1 0 0.00E+00 1.20E+08 2 14 5.83E-08
    HB2 1.20E+08 2 6 2.50E-08 2.40E+08 2 6 1.25E-08
    HB3 2.40E+08 2 4 8.33E-09 4.80E+08 2 4 4.17E-09
          TX Delay 3.4167E-07     RX delay 3.83E-07

    You can see total delay comes around 725 ns almost near to your measured value

    So please read 0x02 and 0x03 registers just to make sure FIR is bypassed?

Children
No Data