Hi,
My customer want to know the response time of AD9361 in MGC mode.
1. In MGC mode, if the gain is increased/decreased by the input pin, what is the response time (i.e. the delay from the end of the control pin enablement to the gain effect) of each gain adjustable module (LMT, LPF, etc.) after the control signal input?
2. In MGC mode, if the gain parameter is written directly through SPI, what is the response time (that is, the delay from the end of the SPI write operation to the gain taking effect) after the SPI write?
Thanks!