Category: Hardware
Product Number: adrv9361-z7035
Software Version: Vivado 2021.1 and Gnu radio 3.8
Hi All,
Currently we are working on a few which is related to Telecommunication where to configure the Registers of AD9361 we are currently using Gnu radio 3.8 by setting the LO Frequency and other required settings for our application but it is observed that there is a LO Frequency Leakage from the Tx of AD9361
PFA Images attached for refference.
The peak is spectrum analyzer is just after GNU Blocks are made to run and even without any signal there is an leakage output being displayed in CRO and Spectrum analyzer
Kindly Provide me a info/solution to resolve this issue