Hi,
I just bought an FMCOMMS5 and ZC702 as the carrier board, I am using analog devices reference design 2019_r2 both for HDL and no-OS. If i build the default ad9361 project (with the default HDL) and debug everything seems to be fine i get the below output:
cf-ad9361-lpc: Successfully initialized (122879028 Hz)
ad9361_init : AD936x Rev 2 successfully initialized
cf-ad9361-dds-core-lpc: Successfully initialized (122879028 Hz)
Done.
When i uncomment the #define FMCOMMS5 line in app_config.h to use the both ad9361 on the fmcomms5 board i get the error below:
cf-ad9361-lpc: Successfully initialized (122880554 Hz)
ad9361_init : AD936x Rev 2 successfully initialized
Calibration TIMEOUT (0x244, 0x80)
ad9361_init : AD936x initialization error
DS24 led on the carrier board is on,
DS301 led on the fmcomms5 (very weak light) on.
Everything is at default and the zc702 and fmcomms5 boards are both new, i could not find a solution in the forum or google, so any answer would be appreciated.
Thx