I have made a boad using AD9363 and ZYNQ.
The AD9363 initilize succefully at the first time when power on and FPGA configuration.
If I run the program again in Xilinx SDK, the UART print as follows:
0:1:2:3:4:5:6:7:8:9:a:b:c:d:e:f: 0:# # # # # # # # # # # # # # # # 1:# # # # # # # # # # # # # # # # ad9361_dig_tune_delay: Tuning RX FAILED!
And there are two spurs below and above the LO:
The spure frequency=f(lo)+/-f(samlping clk)/2