Hey,
We are using a board that has ad9361 on it.
We know that the rx fc is limited to 70 MHz, however we thought perhaps there is a way to recieve at a lower frequency as in the following table
in page 6/72 in ad9364 register map it seems that when the vco is divided by 128 it should reach frequencies lower than 70 MHz.
Also from What limits the lower frequency range to 70MHz?
it seems that they state that the performance at such frequencies was not tested.
What is the method to bypass this limit, even at the cost of performace reduction?
We know that generally speaking we should use a down converter for this task, but we would like to avoid this for now.
Thanks a lot