Post Go back to editing

AD9364 Connection with Raspberry PI

Hello

I consider to connect the AD9364, placed on a custom made board with Raspberry Pi 4 in the following way:

1. Raspberry PI SPI interface will be used for communication with AD9364

2. Raspberry PI GPIO pins will be connected to the AD9364 GPIO pins. A HW conversion to/from 3.3V/1.8V voltage levels will be implemented in HW

Do you see any issue with such implementation?   

Thanks.

  • You can use SPI interface for communication with AD9364.

    Make sure that the setup and hold times are met as per datasheet:

    Note that our chip supports LVDS/CMOS data interface. 

    Raspberry PI GPIO pins will be connected to the AD9364 GPIO pins

    Yes, this can be done

    A HW conversion to/from 3.3V/1.8V voltage levels will be implemented in HW

    Make sure the power supply is able to provide the current specs as mentioned in datasheet.