AD9364: Gain and Decimation Settings

Greetings,

  I have the following questions from our RF busy regarding this device's gain and decimation settings:

  • Can we turn off (or bypass) gain?  (or, can we set the gain to be zero?)
  • Can we turn off (or bypass) decimation?  (or, can we set the decimation factor to be 1?)

We would like to have "flat" gain across all frequencies between the 70MHz minimum up to 2.4 GHz.  

Is this possible?

Our SW setup is a Linux based system, with the ADI R2019 release, using the IIO subsystem functionality.

Thank You in Advance for your time and expertise.

Regards,

Stephen Beckwith