The relationshhip between ad9361 baseband clock chains

In ad9361's driver(2019_R1) software ad9361.c(https://github.com/analogdevicesinc/no-OS/blob/2019_R1/ad9361/sw/ad9361.c), function ad9361_calculate_rf_clock_chain() gives only 7 possible relationships among ADC_FREQ/R2_FREQ/R1_FREQ/CLKRF_FREQ/RX_SAMPL_FREQ:

	const int8_t clk_dividers[][4] = {
		{ 12, 3, 2, 2 },
		{ 8, 2, 2, 2 },
		{ 6, 3, 1, 2 },
		{ 4, 2, 2, 1 },
		{ 3, 3, 1, 1 },
		{ 2, 2, 1, 1 },
		{ 1, 1, 1, 1 },
	};

Is that the only possible choice of baseband clock chains? I'm confused because I also have run Ad9361_Filter_Wizard.m  in matlab which give more choices than it.