AD9361 SPI BUS

Hi all, Is there any possibility to reset the spi bus in ad9361? so that i can start a fresh transaction with AD9361 without reprogramming or switching off the board

  • 0
    •  Analog Employees 
    on Oct 23, 2020 4:00 PM 1 month ago

    Check RESETB
    RESETB is an input signal allowing asynchronous hardware reset of the AD9361. A logic low applied to this pin resets the device (all SPI registers are reset to default settings and the device is placed in SLEEP mode). The RESETB line should be held low for at least 1 μs, and the device should not be programmed for at least 1 μs after the RESETB line has been taken back high.